Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Contraction Tube

Contraction Tube
Sales Price: 0.99 SGD
Review Rating: 4.51
369 Customer Reviews
5 star 264
4 star 51
3 star 39
2 star 7
1 star 8
The reviews are automatic translation.
Showing 1 - 20 of 369 Reviews
As an insulator after soldering between wires
5
From Japan
On 2018-05-24 14:53:40
It is very good that you can freely cut the length according to the application.
This review is about item#18381256.
Maintenance
3
From Japan
On 2018-05-23 18:04:52
It can be used normally. It is feeling that it is neither possible nor impossible.
This review is about item#34608682.
Used for wiring soldering
5
From Japan
On 2018-05-23 17:48:59
The insulation of the partial cover of the solder worked better than I expected.
This review is about item#18381256.
Insulation
5
From Japan
On 2018-05-23 14:37:46
Used for connection between wires. It contracts properly. I'm thankful that you can get something of the same thickness as a monotary.
This review is about item#18381274.
Used for coating after wiring soldering
5
From Japan
On 2018-05-13 19:47:02
Although it can be Giboshi, it was soldered and coated for soldering unnecessary parts. Buy it if it does not buy it.
This review is about item#18381238.
Insulation of electric wire etc.
5
From Japan
On 2018-05-13 14:40:58
I used it for the first time, it is very good. I am satisfied with abundant size expansion and price. It is a shame because it is sold in 1 m unit. We would like to sell long size!
This review is about item#55136393.
For maintenance of electric appliances
3
From Japan
On 2018-04-24 20:57:05
Is it natural for insulation on the solder connection between the wires? ,,, It is inconvenient to peel off or sticky with a vinyl tape. First a little thin thing first and then a bit thick guy I'm covering it on top and doubleing it. I think that it is a good shrinkable tube without being particularly good or bad in terms of quality.
This review is about item#18381247.
Bicycle wire end treatment
5
From Japan
On 2018-04-18 12:49:05
Compared to Sumitube, it is slightly soft and has high transparency. Flexible, is not the protection feeling somewhat inferior? Although there is no quality anxiety, it may be better for you to distinguish depending on usage.
This review is about item#55136375.
Insulation of soldered part
5
From Japan
On 2018-04-16 16:02:59
It can be used as well as a major manufacturer product. Because raw materials are the same, it is natural.
This review is about item#18381247.
Wiring protection
5
From Japan
On 2018-04-15 10:09:55
There is no problem with quality. It is saved if there is sale in longer units.
This review is about item#18381475.
Used for various everyday items
4
From Japan
On 2018-04-13 22:37:19
There is no need to worry if there is a fine size lineup within 10 to 30 mm.
This review is about item#34608716.
Insulation of soldering terminal,
3
From Japan
On 2018-04-12 21:24:10
Very rarely there was a thin wall thickness, but it is roughly good quality.
This review is about item#55136463.
For cable protection
4
From Japan
On 2018-04-11 21:09:14
It is very cheap and good. Although the quality as a shrinkable tube is satisfactory, There are many parts where the folds are strongly attached, depending on the application, it may be a waste.
This review is about item#18381256.
Covering of electrical wiring
5
From Japan
On 2018-04-06 16:27:54
It is very good as the size which is not in the home center is finely grained.
This review is about item#18381238.
For myself
5
From Japan
On 2018-03-30 22:33:13
It is saved because the price is cheap. Easy to use, no problem.
This review is about item#34608673.
Binding of wiring
4
From Japan
On 2018-03-28 15:38:15
It is cheap and fast. It is said that it will be useful in the future as it can be stabilized with the electric heating appliance used now.
This review is about item#18381265.
Cable protection after soldering
5
From Japan
On 2018-03-25 14:30:45
I often chew. Glossy material. It can be constructed immediately with a lighter. no problem.
This review is about item#18381274.
Wiring repair
5
From Japan
On 2018-03-24 17:37:01
Because it is rose sale, since price is cheap, it is saved, use impression is also good.
This review is about item#18381283.
Electronic circuits and electrical wiring
5
From Japan
On 2018-03-20 14:45:41
There was electronic circuit creation for the first time in a long time, and I used it. It was easy and easy to use than I expected.
This review is about item#18381238.
On the soldered part of the switch wiring of the motorcycle
3
From Japan
On 2018-03-09 06:16:07
It is okay. It melts a little if it heats up a little ,,,.
This review is about item#34608673.
Customer Who Viewed This Item Also Viewed
Heat Shrinkable Tubing, General Use, Transparent
Shrink Tube3phi
Large Diameter Shrinking Tube
Raychem, RaychemContraction Tube V2
Heat Contraction Tube
Heat Shrink Tube
Shrinkable tube 5 phi
Contraction Tube 2phi
High Shrinkage Tube, 4:1
High Shrinkage Tube, 3:1
Heat-Shrinkable Tube F, Z
Heat-Shrinkable Tube A
Heat Shrinkable Tubing, General Use, Black
Heat-Shrinkable Tube A
High-shrink tubing (4: 1)
Color Shrink Tube, Red
Contraction Tube
Contraction Tube