Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Snap Off Knife, L type

Snap Off Knife, L type
Sales Price: 7.98 SGD
Review Rating: 4.90
10 Customer Reviews
5 star 9
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
For cutting of PP board etc
4
From Japan
On 2017-05-06 12:10:44
It is a staple item. Moreover, it is representative famous manufacturer. Until now, I was cheating with an ordinary cutter, but I anticipate that the cutting work of the PP board will increase, so I will purchase it. This L type, small type, similar products of other companies, I got lost a little, but I decided on this L type made by Olfa. It is overwhelmingly easy to use. It is powerful and the work efficiency has been significantly improved. It seems that it got easier to grasp, easy to put in force, replacement blade storage mechanism, model changed a few years ago. However, there are some difficulties enumerated. 1) Small machining and small R can not be cut. Even though I can do it, it is painful to do. So, depending on the situation, "Olfa Art Knife" https://www.monotaro.com/g/00137994/ "Belt punch" similar to https://www.monotaro.com/g/01271541/ distinguishably used I will. Also, similar to "Circle cutting cutter" https://www.monotaro.com/s/c-123666/ Type of "Curve cutting template" (It seems that it is not handled by Monotaro, so I request it from inquiries I want it, but I have not obtained it yet. ... Anyway, I wonder what to buy. ← I think that this person. ☆ ☆ ☆ 2) Unless you set the tip on the front side and the guide on the other side, it is difficult to understand the position where the tip is hit. Although it may be useless, I try to design and arrange it so that I can cut it too much. (Although some material is wasted, it will be so if efficiency is given priority.) 3) The cutting depth does not become uniform. This may be a problem of workmanship, but both ends of the cutting line are shallow and only deeper, such as "rowing a ship". In other words, before it is completely cut off, the one in the line pierces the material and scrapes the lower base (cutter mat etc). So, when you can penetrate a part of the interim, the rest is not separated from this P cutter, but it is separated by a conventional ordinary cutter or the above art knife etc. (Since the material is thinned, it is easy to cut even if it is not a P knife and the grooves are already made, so the cutting line is hard to bend without using a guide.) It is difficult to use several instruments depending on the situation It seems to be the best. This P cutter is one of its useful instruments.
This review is about item#34621431.
To cut a 0.5 mm brass plate
5
From Japan
On 2017-03-15 19:45:34
A very handful fitted and a blade with a crochet shaped shape was sharpened firmly. If it does not scrape to about half, it is hard to fold, but because it comes with 2 blades in spare, you can work immediately.
This review is about item#34621431.
Cutting of laminate board for forehead
5
From Japan
On 2016-10-08 09:59:44
It was easy to use and was well off.
This review is about item#34621431.
Panel cutting
5
From Japan
On 2015-08-01 15:11:38
It was quite easy to cut. It may be better to change the blade after use
This review is about item#34621431.
To cut PVC board
5
From Japan
On 2015-01-29 16:48:28
I am satisfied with the sharpness being good
This review is about item#34621431.
Acrylic sheet cutting
5
From Japan
On 2014-11-09 17:31:34
Because the acrylic board to be cut was 5 mm thick, I thought this model was suitable.
This review is about item#34621431.
Acrylic cutting with 5 mm pressure
5
From Japan
On 2014-08-23 22:39:19
Using an acrylic plate of 5 mm pressure as an alternative to breakage of the sash window of 800 mm × 1100 mm, the budget is half of the usual and the weight is a bit lighter compared to the glass, so there is a danger that the wind is blown by the wind I finished stabilizing the window with adjustment, completed cutting the hand with the cutter, could not cut it, I felt memorized my memories of confidence, I felt the way of cutting this place long, but after finding a knack I could cut it cleanly very quickly, The feeling that the cutting edge is small in proportion to breakage is exactly amazing!
This review is about item#34621431.
Acrylic plate cut
5
From Japan
On 2014-07-22 08:42:16
I purchased it because it seems easy to use because it has a big handful. The degree of power input is much better than the conventional small object. It will not hurt your hands even if you cut this number. I should have bought more quickly.
This review is about item#34621431.
I use it for a little acrylic cut.
5
From Japan
On 2014-06-11 13:40:33
Sharpness is also good, and it is comfortable cutting.
This review is about item#34621431.
Cutting of polycarbonate board
5
From Japan
On 2013-10-23 14:40:55
It is very useful because it can store the blade
This review is about item#34621431.
1
Customer Who Viewed This Item Also Viewed
Cutter Blade
Plastic Cutter
Plastic Cutter
Plastic Utility Knife
Snap Off Knife
Snap Off Hook Knife, L type
Utility Knife Blade
Plastic Cutter
Akurisande cutter