Buy more than* S$200* and get FREE SHIPPING
Due to the national holidays as Golden Week, we will close 2018/4/28~2018/4/30 and 2018/5/3~2018/5/6.
This may cause delays with our responses. Thank you for your understanding.

Customer Reviews of Delta drill bit SDS and plus (delta axis)

Delta drill bit SDS and plus (delta axis)
Sales Price: 10.99 SGD
Review Rating: 4.92
12 Customer Reviews
5 star 11
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 12 of 12 Reviews
Drilling for split pins
5
From Japan
On 2017-04-20 21:18:21
The triangle of the tip helps to drill in the correct position.
This review is about item#6651294.
Drilling of stone and concrete during electric construction
5
From Japan
On 2017-01-30 18:35:22
There will be no displacement of the hole position, it will go straight. Durability seems to be good. Since I trust it, I use this hammer drill only for this manufacturer.
This review is about item#6651233.
Drilling of concrete screws
4
From Japan
On 2017-01-02 00:02:23
If you use it too hard it will bend soon. It is a long-lasting trick to use gently without turning too much.
This review is about item#6651233.
Drilling of concrete skeleton
5
From Japan
On 2016-07-16 00:19:46
Although it is used for fixation of piping etc, the hole opens well. There is no shaking of the core, it is very good. I always use this.
This review is about item#06651303.
Weak electric construction
5
From Japan
On 2015-09-04 17:05:46
It is cheap and shipping is also early so it will be helpful
This review is about item#08738405.
Used for drilling concrete
5
From Japan
On 2013-12-16 00:05:14
I like it because it is delta shape so thin even if it is thin (3.2 mm).
This review is about item#08738405.
Using a non-plug screw to support the piping band
5
From Japan
On 2013-10-14 08:40:19
Because of the delta axis, there is little bending, I think that it can be used for a long time.
This review is about item#06651224.
Drilling for non-ravis
5
From Japan
On 2013-05-13 19:06:34
I always use the delta axis, but it is handy because it lasts long. It is attractive that the price is cheaper than other stores! I will also purchase it.
This review is about item#06651224.
Installation of the instrument to the wall
5
From Japan
On 2013-04-19 10:26:02
I have used it for a long time, but it is very easy to use, and it is difficult for the core to shake.
This review is about item#06651233.
Drilling to the building outer wall
5
From Japan
On 2013-01-21 19:47:57
Chatter discharge on the delta axis is comfortable and it does not chew it In and out of the drill becomes almost useless Roundness is no problem There is no problem with 5 packs · 10 boxes etc. It is better to become cheaper
This review is about item#06651267.
To fix the piping of piping construction
5
From Japan
On 2011-01-23 19:08:54
Holding of the blade is different from other companies.
This review is about item#06651224.
Drilling in concrete
5
From Japan
On 2010-01-13 12:31:56
Miyanaga delta Gonbit is used earlier because it can drill lightly faster than normal bit. I will buy this price!
This review is about item#06651242.
1