Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Thick Saddle

Thick Saddle
Sales Price: 1.99 SGD
Review Rating: 3.17
6 Customer Reviews
5 star 2
4 star 1
3 star 1
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Ventilation fan VP 150 duct fitting
3
From Japan
On 2016-06-11 20:01:17
Normally used as a fixing metal fitting for domestic ventilation fan vp 150 mm. Fastening metal fitting hole diameter is too large so I think it may be a little smaller (used for stopping with wood)
This review is about item#34926552.
To attach the signboard to the curved mirror
5
From Japan
On 2016-04-30 22:12:59
It was easy to fix as width and thickness were appropriate and firm.
This review is about item#34926534.
Supporting and fixing of piping
1
From Japan
On 2015-05-22 15:07:56
I do not understand well with the photograph, but the screw hole is too big to use at all. It seems to be usable if fixed with all screws or anchors, but can not be fixed with ordinary screws. It was trial buying, but 4 pieces are probably useless. I think that there are not many people using such a band. If it is small, you can make it big, but if it is too big you can fix it if washer is used, but I do not have such a big thing. I was disappointed.
This review is about item#34926543.
Used to fix water leakage gutter.
4
From Japan
On 2014-10-30 18:51:13
If there is a danger of corrosion due to water leakage, I think that it is good if there is a stainless steel material.
This review is about item#34926534.
Bellows pipe stopper with external shape 65 mm 7
1
From Japan
On 2013-06-21 19:25:20
Dimensions did not match
This review is about item#34926534.
Plumbing fixation
5
From Japan
On 2013-05-07 16:29:37
It is helpful to be able to purchase fewer items of redcurrants.
This review is about item#34926543.
1
Customer Who Viewed This Item Also Viewed
Support Bracket Saddle
Saddle Band
High Flex Through Saddle
Stainless Steel Saddle Band
Thickness Saddle Band
Stainless Steel Saddle Band
U Clamp
Saddle band
Half Saddle
Saddle Clamp
Saddle (for thick steel)
Saddle Band
Stainless Steel Saddle Band