Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Hinge Type Vertical Band

Hinge Type Vertical Band
Sales Price: 1.99 SGD
Review Rating: 4.43
7 Customer Reviews
5 star 5
4 star 0
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Used for air hose piping
From Japan
On 2017-11-14 16:50:27
It was inexpensive, satisfied, and the strength was satisfying Used for piping pipe of Ich-inch
This review is about item#34927584.
Plumbing fixation
From Japan
On 2017-03-26 19:29:00
There is no problem, you can use it with confidence. It is good to prevent bolt turning around! .
This review is about item#34927593.
Used for detour piping of clogged gutter
From Japan
On 2016-07-04 18:05:48
Workability was good because the bolt does not fall at the time of installation
This review is about item#34927645.
From Japan
On 2016-03-05 23:14:58
Easy to use
This review is about item#34927654.
Bicycle light installation
From Japan
On 2015-07-08 01:33:39
I bought an unused item. Although the thing with a band inner diameter of 40 mm was necessary, it is written as nominal diameter (A) 40, conforming pipe outer diameter (Φ mm) 48.6, which is not clear as to which size is correct, When ordered, the nominal diameter (A) was 46.8 ~ 47.8. If such a description is made, there is a possibility of buying unused items. Please do something. When purchasing, please purchase by looking at the outer diameter of the applicable pipe.
This review is about item#34927602.
Shared rain gutter became unsupported and replaced
From Japan
On 2014-02-28 01:24:41
Originally it was broken by plastic so replace it with this durable iron so that it is perfectly comfortable to use with all dimensions and holes.
This review is about item#34927636.
Supply tube support of sewer
From Japan
On 2010-10-01 21:46:04
Although I had a stay, I bought it because it has gone bad. It is cheap and there is nothing to say.
This review is about item#34927645.