Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Pull Spring Material Stainless Steel SUS304

Pull Spring Material Stainless Steel SUS304
Sales Price: 2.99 SGD
Review Rating: 4.00
10 Customer Reviews
5 star 4
4 star 4
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
For pigeon removal
4
From Japan
On 2018-02-15 16:33:50
I used it last time and could use it normally. . . .
This review is about item#35052911.
My own machine
4
From Japan
On 2017-11-19 19:42:21
The tension of the spring bought to make a life-like machine. When I actually touched it I was relieved that I found enough.
This review is about item#35052857.
Motorcycle scarf
4
From Japan
On 2017-06-14 18:26:23
I used it to fix the connection of the muffler of the motorcycle. I hope there are lots of repertoires of size and strength. Because it is stainless steel, it is suitable for outdoor use.
This review is about item#35052902.
For exchanging springs attached to equipment
4
From Japan
On 2017-03-03 20:17:34
I ordered it by mistake in length, so it was a bit short but it was fully usable. I was sent immediately, so I thought the shipping procedure was excellent.
This review is about item#35052796.
Parts of my own work.
3
From Japan
On 2016-11-08 18:22:34
The information on the details is small, I bought it almost by the image. Spring is stronger than expected and impression that it does not stretch too much. Also, I do not know how long it will be extended, so I can not give you a good load. I think that it will be a very useful reference when choosing a spring constant or limit value.
This review is about item#35052893.
To trigger a toy
5
From Japan
On 2016-10-21 18:18:13
I like it very much. I'd like to order additional items soon.
This review is about item#35052814.
Steel work
1
From Japan
On 2016-09-06 18:01:23
I did not mention it because I did not mention spring constant.
This review is about item#35052936.
Prevention of muffler fall
5
From Japan
On 2016-02-25 15:58:51
It resists strong vibrations and is also resistant to corrosion! The length of the spring part of S-080-03 is 35 mm.
This review is about item#35052902.
This part of a circle
5
From Japan
On 2015-10-06 20:30:22
The pulling force was weak. It was a mistake in selection.
This review is about item#35052857.
Equipment developed in-house
5
From Japan
On 2013-07-15 19:24:24
It is appreciated if there is description of maximum load, spring constant, etc.
This review is about item#35052857.
1