Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Push Spring Material Stainless Steel SUS304

Push Spring Material Stainless Steel SUS304
Sales Price: 2.99 SGD
Review Rating: 4.17
6 Customer Reviews
5 star 3
4 star 2
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Mechanical repair
5
From Japan
On 2016-03-08 23:43:25
I wonder if it was a bit hard. But it was useless because it was purchased as a general purpose item. I do not know because I do not know if I buy online purchase. I failed this time. Things are good.
This review is about item#35053042.
Toy science teaching materials
5
From Japan
On 2015-06-16 15:03:30
The toy showed the expected movement and succeeded. It is convenient that only screws with a diameter of 2 mm and a length of 10 mm are inserted and fixed. Also, I want something with some spring characteristics. It is promising as a material of monozukuri teaching materials this time.
This review is about item#35052945.
Brush repair of disc grinder
4
From Japan
On 2014-06-29 23:49:01
It is used for repairing Ryobi's disc grinder nearly 30 years ago. The spring of the carbon brush is burned out due to overload and the brush assembly for repair is also abolished, cut this spring close to the wire diameter and the number of turns, wind it around the brush wire and replace only the spring, burn it The brush surface was repaired a little with a hook to complete repair. When the brush is completely gone this time, it may be a lifetime to drift, but I think that it will be able to work hard with active for a while now.
This review is about item#35052972.
Spring of nipper
2
From Japan
On 2012-10-25 13:38:28
Springs of plastic nippers break or lose as they break apart. Because the dedicated spring was expensive, I purchased this product. But it seemed that the strength was insufficient. I wish there were variations in strength even with the same diameter.
This review is about item#35052954.
Repair of entrance key
5
From Japan
On 2012-10-19 12:29:02
Part of the entrance door that had been broken for many years revived by exchanging the springs Parts like this are not very useful in town,
This review is about item#35052997.
Spring buffer elasticity
4
From Japan
On 2012-03-01 20:16:43
There was something similar to the home center in the neighborhood, but the finish of the surface was beautiful here. I am sorry that the length is determined by the standard or there is no spring with a free length of 70 mm or more.
This review is about item#35053006.
1