Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of U-Shaped Socket

U-Shaped Socket
Sales Price: 4.99 SGD
Review Rating: 5.00
3 Customer Reviews
5 star 3
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
In case of laundry clothes raft
5
From Japan
On 2017-06-09 20:31:21
In the rainy season no laundry, when I wash clothes, I received a clothespin, the width of reception is great, so it is easy to receive the pole and it is handy. If you have a stopper in the horizontal direction (not in the upward direction) to prevent the falling of the rod, I think it is more useful.
This review is about item#35063752.
As a stainless steel pipe holder of clothespin
5
From Japan
On 2016-03-24 19:00:33
Even amateurs were easy to handle and the quality was also good.
This review is about item#35063752.
For earthquake resistance, furniture toppling prevention. Fixed through stainless steel pipe.
5
From Japan
On 2015-05-03 16:14:02
If it is a solid wall it is definitely this. This is good if you can change the function of the room because you can remove the pipe with one touch. It is unsuitable for weak walls, so it is best to have a hook with a flange in the future ...
This review is about item#35063752.
1
Customer Who Viewed This Item Also Viewed
SUS One-Touch Socket
Pipe Socket Screw Type
Brass Pipe Chrome Double Socket
Lumina socket
Easy Socket Screw Type
DC Chrome U-Socket
Complete socket
Double socket
Oval Pipe Socket
One-touch pipe support
Complete Socket
Pipe support
New U type complete socket
U-shaped socket