Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Large Diameter Shrinking Tube

Large Diameter Shrinking Tube
Sales Price: 7.99 SGD
Review Rating: 4.67
63 Customer Reviews
5 star 47
4 star 11
3 star 5
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 20 of 63 Reviews
Protection of piped tight seal
5
From Japan
On 2018-01-04 16:20:45
It protects it so as not to lose it by peeling it over the name seal of various parts.
This review is about item#35072116.
Production of amateur radio antenna for car
5
From Japan
On 2017-07-31 19:40:20
Excellent durability (rain, snow, ultraviolet rays, etc.) It is easy to produce wireless antennas.
This review is about item#35072247.
Easy case of electronic parts
5
From Japan
On 2017-04-29 20:31:18
Purchased for easy insulation of electronic components. Even if there is somewhat unevenness it will wrap tightly without tearing and it will look somewhat whitish but if it is about the emission of LED. Because there is flexibility, if you place the tact switch if you think about height, you can not press it.
This review is about item#35072177.
As a protective cover for fishing rods
5
From Japan
On 2017-03-21 19:53:52
In addition to using it as an insulator for electrical construction, it is also used for waterproofing and prevention of hobby fishing rods. Because the shrinkage due to heat is large, it fits in the form of concavities and convexity, it can be used forever and it is very handy.
This review is about item#35072292.
Waterproof plug cover
5
From Japan
On 2017-03-05 16:52:42
It is used instead of the taping of the rubber part of the pushbutton switch rubber cap and the cap tire, the taping of the middle part of the cable, durability is more than the taping, and it is more durable by overlapping it.
This review is about item#35072283.
Production of self-made antenna of amateur radio
4
From Japan
On 2017-01-26 21:01:26
For goods you can use it without problems but I think that it is easier to use if there is a product with half the wall thickness if possible.
This review is about item#35072283.
Used to gather audio cables.
5
From Japan
On 2016-12-21 16:34:09
I use it to gather the audio pin cables and earth. It is well organized.
This review is about item#35072222.
Dustproof construction machine
5
From Japan
On 2016-11-18 15:43:42
In the last time, it was troubled that φ30 (black) disappeared. It is useful for revival. (Instead of using φ40, the amount of contraction was too much and it took time.) Φ40 → φ30)
This review is about item#35072301.
Bundle the code
5
From Japan
On 2016-10-31 16:32:45
Since the shrinkage ratio is large, it is good that it can correspond to various diameters
This review is about item#35072256.
Terminal treatment of rope
5
From Japan
On 2016-10-05 10:24:01
I used it for the end treatment of the rope of 12.5 m. After trying to shrink it with the heat gun, it got on firmly. There is strength, too. Because it contains a lot, it can be used for a while.
This review is about item#35072231.
When the electric wire is fixed in a portion with vibration
4
From Japan
On 2016-09-30 12:44:56
Since it has a relatively large inner diameter and can be shaped by heat, it is useful for wire protection of the vibration part.
This review is about item#35072256.
Protection of lures
5
From Japan
On 2016-07-19 01:27:04
Used to protect the lure (metal jig). Painted lures of the lure can be prevented and durability can be improved.
This review is about item#35072091.
Machine modification
5
From Japan
On 2016-06-23 17:15:09
Ideal for reinforcement of wiring etc.
This review is about item#35072091.
Processing of electric appliances
5
From Japan
On 2016-05-08 20:53:24
Finish is beautiful
This review is about item#35072326.
Used for fixing the guide tube.
5
From Japan
On 2016-05-03 07:53:16
There are many things that can not be passed without removing the banjo adapter for the guide tube attached to the front brake hose of the off - road motorcycle, but it was possible to pass this item as it is installed. Because the shrinkage rate was also high, it was able to stop it neatly.
This review is about item#35072125.
Used for RC work
5
From Japan
On 2016-04-18 19:41:47
It is an excellent product with high quality. I was surprised to see that 1 m × 5 bottles had not arrived because the pins did not come.
This review is about item#35072213.
Rust prevention for steel bars
5
From Japan
On 2016-03-26 14:45:26
It worked well.
This review is about item#35072256.
Koukann
5
From Japan
On 2016-03-09 20:36:25
Iiyo
This review is about item#35072082.
Cover connection
3
From Japan
On 2016-03-02 18:18:40
I attempted to shrink with a hairdryer but it was useless.
This review is about item#35072091.
We are using for making speaker cables etc.
5
From Japan
On 2016-01-16 21:45:05
I am using it to create a speaker cable etc., but I think that I want to use it again because it is very easy to use and shrinks cleanly.
This review is about item#35072152.
Customer Who Viewed This Item Also Viewed
Heat Shrinkable Tubing, General Use, Transparent
High Shrinkage Tube, 3:1
High Shrinkage Tube, 4:1
Heat-Shrinkable Tube F, Z
Heat Shrink Tube
Contraction Tube
Heat-Shrinkable Tube A
Heat Shrink Tube, UL Standard Product
Heat Shrinkable Tubing, General Use, Black
Heat-Shrinkable Tube A
Shrinkable tube 6 : 1
Heat shrinkable tube
FEP Heat Shrinkable Tube
Color Shrink Tube, Red
Heat Shrink Tubing TFE
Heat shrinkable tube 1m goods (black)
Heat-Shrinkable Tubing
NPE Heat Shrink Tubing