Buy more than* S$200* and get FREE SHIPPING
Due to the national holidays as Golden Week, we will close 2018/4/28~2018/4/30 and 2018/5/3~2018/5/6.
This may cause delays with our responses. Thank you for your understanding.

Customer Reviews of Hexagonal Shaft Spiral Taps

Hexagonal Shaft Spiral Taps
Sales Price: 4.99 SGD
Review Rating: 4.12
83 Customer Reviews
5 star 46
4 star 17
3 star 10
2 star 4
1 star 6
The reviews are automatic translation.
Showing 1 - 20 of 83 Reviews
For processing aluminum sash
5
From Japan
On 2018-04-23 14:37:39
Combination of aluminum sashes The impression I used to make the door of simple greenhouse is that it is easy for the opponent to cut the tap with aluminum, but even if it cuts too deeply it will wobble and the screw hole will stagger and the screws are totally useless Although it is gone, I got used to it several times while I was doing it.
This review is about item#35099391.
Tap on steel plate
4
From Japan
On 2018-02-17 21:52:20
Used for tapping 3 mm screw to 3 mm steel plate. There is no problem in sharpness, there is nothing of a trimmed, but with the first eclipse It is repulsed. Because it is M3, it is likely to break if it is impossible with a drilling machine, I went by hand work.
This review is about item#35099391.
Tap off the screw hole
5
From Japan
On 2017-12-15 09:53:48
Because I was cheap, I was worried that I could break easily, but I could use it just like a maker's item as before. Because it is a hexagon, it will not slip. It can also be used for electric tools, it can be used as a hand-held driver to insert a hexagonal axis, and it can be used manually, which is very convenient. I used it quite a bit, but as of now I have not broken one.
This review is about item#35099391.
Onsite drilling work
5
From Japan
On 2017-10-07 20:51:42
Purchase because it is easy to use and used by other people from before I tried using it, it was as good as another company's expensive one
This review is about item#35099425.
EC mounting
1
From Japan
On 2017-09-05 03:01:12
Purchased because it is cheap. Iron plate 2.3 mm (pilot hole 4.2) It broke at the sixth time from the new article by M5 thread processing. Quenching is hard to the center of the tap, the spiral is deep.
This review is about item#35099416.
Tapping on aluminum frame
1
From Japan
On 2017-06-07 16:36:17
I needed a screw hole about 1 cm in length. Whether the fixation of the work is insufficient, the impact driver 's torque setting is not good, or whether I'm clumsy or not, the reason is not somewhat, but it fell into the pilot with a single shot and it broke back and the work became unusable. I broke the broken tap.
This review is about item#35099407.
For tapping
5
From Japan
On 2017-04-23 14:56:58
Cost performance is the best. I also want to buy it.
This review is about item#35099416.
Make screw threads on iron materials etc.
5
From Japan
On 2017-04-23 01:08:39
It is convenient because it allows you to make screw threads in a short time, it is also cheaper than other companies.
This review is about item#35099425.
When working jig production
2
From Japan
On 2017-04-02 19:47:13
There were variations in the dimensions of the hexagonal axis and it was hard to remove.
This review is about item#35099416.
I use it where I can not install the nut.
4
From Japan
On 2017-03-28 09:31:19
I am satisfied with sharpness well. I am happy if there is also a No. 2 tap.
This review is about item#35099391.
Tap drilling work
5
From Japan
On 2017-02-23 19:52:34
Also purchased for M5. Since size entry is printing, it disappears soon and it becomes impossible to know whether it is M5 or M6. Although M4 is truly thin, it is distinguished though ....
This review is about item#35099425.
Tap processing
1
From Japan
On 2017-02-02 06:07:40
I bought other sizes, but the hexagonal axis part does not enter only this size, it is the situation that it can not come out. As it is cheap, the accuracy seems to be secondary. There is a part I am sorry to think that I have to cut it out for a cheap part.
This review is about item#35099425.
Used for repairing and processing machinery.
5
From Japan
On 2017-01-17 14:50:29
After the pilot hole processing of PL 6 (φ 8.5), direct tapping processing was possible without using 1st tap.
This review is about item#35099443.
Control panel assembly
3
From Japan
On 2016-12-31 16:58:25
I think that it is cheap but good compared to other taps, it is magnetized and it seems easy to get a trim.
This review is about item#35099407.
Control panel assembly
5
From Japan
On 2016-12-20 20:12:56
Price is cheap and sharp. I worked about 50 holes, but I can still use it.
This review is about item#35099407.
Electromechanical maintenance
4
From Japan
On 2016-11-19 12:03:15
it is normal. It can be used normally, it is cheap normally. Since it is a consumable item in the first place, I think that it is worth buying just that it can be used normally and cheaply and disposable
This review is about item#35099391.
Control board creation
5
From Japan
On 2016-11-05 20:41:59
I am using it without particular problem. Sharpness is also reasonable.
This review is about item#35099425.
Electric wiring
4
From Japan
On 2016-07-29 17:48:55
There is no problem in initial use. Durability in long-term use is unknown.
This review is about item#35099407.
Local work
5
From Japan
On 2016-06-04 15:25:19
I have this hexagonal shaft spiral tap, but I bought it as a spare when it broke. Sharpness can be used well without problems.
This review is about item#35099407.
Hole drilling of sash
5
From Japan
On 2016-03-09 19:03:10
The price was cheap but the price was equivalent to the ones above.
This review is about item#35099407.
Customer Who Viewed This Item Also Viewed
No.28 Hexagonal Shaft Tap
Point Threading Tap
No.28-S Hexagonal Shaft Spiral Tap
Hex Shank Taps
Hexagon-head axis spiral fluted tap
Hex Shank Tapping Drill
Spiral tap
Hex Axis Drill Tap