Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Wastewater Pump

Wastewater Pump
Sales Price: 309.99 SGD
Review Rating: 3.75
4 Customer Reviews
5 star 2
4 star 1
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
The spring water of the basement. . . For automatic drainage
5
From Japan
On 2017-11-09 15:24:36
This pump is. . There is power, even stone pachinko balls will be discharged without problems. . . However, if you do not make the water distribution pipe a bit thicker, it is a small one such as reverse discharge valve. . Attention is necessary because piping is clogged first with mud and impurities Hose etc. If connected directly. . . It discharges pleasantly Even a full bath will be pumped up in the blink of an eye. . .
This review is about item#35143744.
Automatic drainage of the drainage of the septic tank
5
From Japan
On 2015-06-03 22:14:18
I am very satisfied. Up to now, I had to work on the drainage work after visual inspection, but since it can be drained automatically, it is helpful for preventing unnecessary work, backflow to the septic tank, I am very satisfied, Thank you It was very satisfying, especially price
This review is about item#35143744.
Used for draining rainwater collected in fields
4
From Japan
On 2015-04-07 14:24:35
Because the float of the pump which was used before was spherical, it was often that it caught in a narrow sump well. However, since the float of this time moves linearly up and down, switch operation is good even with a small sump.
This review is about item#35143744.
Pumping sewage sewage
1
From Japan
On 2013-06-11 07:55:36
Inferior goods not extraordinary. Problem with initial assembly. Because I did not pump it up for the first time in water so scratchy and surprised. The bolt stopping the feather was falling. It is unclear whether there is no bolt and washer whether the tightening is forgotten or whether the tightening was sweet. Installing substitute bolts while being covered with sewage. The beginning of the day was the worst day. Tsurumi pump was shocked just because I trusted.
1
Customer Who Viewed This Item Also Viewed
Sludge Submersible Pump
General Dewatering Pump HS
Sludge Submersible Pump, Light Resin
Sludge Submersible Pump, Light Resin
Submersible Pump, Construction
Submersible Pump Compact
Submersible pump for filth
Underwater Pump
Submersible Sewage Pump
Submersible pump bank series for sewage
Sewage Pump
Submersible Pump, Ponster
Submersible Pump, Ponster
General Dewatering Pump LB