Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of SR Threaded Caster

SR Threaded Caster
Sales Price: 4.99 SGD
Review Rating: 4.40
5 Customer Reviews
5 star 2
4 star 3
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Replacing the broken baby cribs caster
5
From Japan
On 2017-09-27 23:01:44
Because the caster's resin press fitting wheel part broke, I attached it to a baby bed in combination with an adjuster base. Both strength and motion have no problem, and it has become a natural finish.
This review is about item#40263316.
Replacement of casters damaged items on tables with casters
5
From Japan
On 2017-05-15 10:36:55
The inch screw casters were not in the nearest DIY shop, but the same item was ordered immediately in your catalog. I arrived there two days later and was extremely helpful. The elastomer wheel is familiar to the floor better than the damaged plastic one and I am very satisfied.
This review is about item#40263334.
For self-made tool wagon
4
From Japan
On 2016-05-30 09:51:58
I waited for about a month in stock but it was worth waiting for goods to deal with the person in charge of "Monotaro" as well. I'd like to expect durability which made this type thinking about various wheel types.
This review is about item#40263334.
Used as a substitute for home folding beds
4
From Japan
On 2015-08-03 18:22:40
Castors for the folding bed for home did not snap into the carpet well. After exchanging for this caster, it moves smoothly. The casters that came with the bud work well with flooring, but with tatami and carpets, I think that it was good to be buried and not move and exchange. It is going smoothly.
This review is about item#40263352.
For moving industrial machinery
4
From Japan
On 2013-05-28 00:05:25
Because I wanted to check with an image because it is a material that is not a major in the price range with an elastomer wheel, I decided it was cheap, but it was cheap. There is a feeling with a little groundering in the bearing and it is poorly accurate, but still it is this price ... · · ·. The wheels are not too hard, they are not too soft and they do not trace on the floor, so it feels good. However, as I mentioned earlier, the accuracy of the ball bearing is not good, so it would be wise to use it after greasing if there is no problem with the installation location. It is better not to expect it because it is like a toy with a structure that stops by stopping the stopper by pinching the wheel. If you use the stopper function too much, it seems that the wheels are likely to rattle. At any rate, there are no complaints as it is cheap.
This review is about item#40263316.
1
Customer Who Viewed This Item Also Viewed
SR Threaded Caster
Swivel Caster, Stopper
Double outlet with a ground with a flat earth terminal
Gold Screw-In Caster