Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Nylon Flat Belt, Drum Wind

Nylon Flat Belt, Drum Wind
Sales Price: 77.99 SGD
Review Rating: 5.00
3 Customer Reviews
5 star 3
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
For fixing in the car or
5
From Japan
On 2017-04-12 15:09:58
I was worried whether the thickness would fit the buckles on hand, but it could be used without problems. First of all, the belt of my pants. Next, I'm thinking about fixing belts for car luggage. I was wondering whether to make it black or gray, but it was gray and was the correct answer.
This review is about item#35214304.
Door opening and closing support
5
From Japan
On 2016-07-03 18:31:07
It was a workable material.
This review is about item#35214295.
Anti-earthquake measures on shelves
5
From Japan
On 2014-09-26 18:53:48
I used it in combination with an adhesive pad to fix the shelf and the wall. The band has a firm thickness, and there is a sense of security very strongly, but when you want to pass through a narrow gap it may be minus. Compatibility with the same manufacturer's "TRIGLIGHT 25 mm" is compatible and firmly stops. Since the drum can remove the upper and lower disks, when using a lot, I use one disk to remove it. Although it is a serpent, if you leave it, the edge gets frayed, but if you smash it quickly with a gas burner or a lighter, the thread melts and it will stop fraying.
This review is about item#35214304.
1
Customer Who Viewed This Item Also Viewed
Flat Belts
Flat Belt Fitting
PP Belts
Bracket C buckle
Metal Ladder Lock
PP Belts
PP Belts
Bracket plate Feed 25mm
A Buckle
Flat belt acrylic color