Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Slide-Type Ring Spanner

Slide-Type Ring Spanner
Sales Price: -
Review Rating: 4.17
6 Customer Reviews
5 star 3
4 star 1
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
For maintenance of motorcycle
4
From Japan
On 2017-01-14 17:41:22
It is possible to change the size, because it is thinner than I thought, it really helps if you own two or more bikes of different sizes.
This review is about item#35226633.
motorcycle
3
From Japan
On 2015-01-14 18:12:34
I'd like to have an angle because it is a narrow wrench. But strength is good
This review is about item#35226633.
For motorcycle maintenance
5
From Japan
On 2014-07-16 15:25:52
I own various types of bikes from on to off, so these products are really helpful. We can use it for motorcycles from 125 cc to 1000 cc.
This review is about item#35226633.
Bike suspension adjustment
5
From Japan
On 2014-02-18 13:08:14
I bought it so it arrived soon so it was good. The product was also very easy to use, and it was a thing of purchase value as a product. Just thinking about price makes me feel high. I think that it may be cheaper by about 1000 yen.
This review is about item#35226633.
Stem nut adjustment
3
From Japan
On 2012-08-22 22:12:14
I can not use it for the stem nut in the car - mounted pin spanner, so I bought it because it can be used for both stem and rear suspensions for this product. It looks pretty cheap as a tool but it is easier to use and easier to adjust the rear suspension that requires the power than the on-board tool, and I think that I was able to buy a steering wheel that had a backlash, so I was glad I bought it for the time being . However, people who are committed to tools may prefer to choose something of higher quality.
This review is about item#35226633.
Tightening of bike stem, suspension lock nut, bearing nut etc.
5
From Japan
On 2012-07-01 01:05:30
Although I have several normal hook wrenches, there are several times that application diameters do not match when it comes to use, and since I bought a wrench every time, wrenches that use less frequently increased at the bottom of the tool box I just got to go. This time I decided to buy this adjustable wrench from 35 to 75 mm. Hook the nut on the lock nut and rotate the worm gear to apply the handle to the nut and use it normally. Also, since the 9.52 mm square hole is open in the handle, it seems that you are also considering using 3/8 torque wrench. There seems to be no further wrench increase anymore.
This review is about item#35226633.
1
Customer Who Viewed This Item Also Viewed
Connection spanner
FP hook pin spanner
Hook Wrench
Freely hook wrench
Flexible hook wrench
Pin Spanner
C Spanner
Sliding adjustment hook spanner
Hook wrench
SW Condor Handle