Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Spot Drill

Spot Drill
Sales Price: 7.99 SGD
Review Rating: 4.18
11 Customer Reviews
5 star 8
4 star 0
3 star 1
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
Bottom surface treatment of blind hole
5
From Japan
On 2017-10-23 22:14:35
Originally we used the tip of the drill blade with a grinder to scrape off, but since we began using this drill blade, the treated surface finished cleanly.
This review is about item#35265474.
Drilling of copper plate
5
From Japan
On 2017-10-22 20:14:12
Better sharpness than the base, burrs in the hole without finish was good.
This review is about item#35265361.
Used for non-penetrating hole of self-made case tap screw hole
3
From Japan
On 2016-10-14 15:15:17
I bought the item at the local home center, but if the drill stopper is also set, adjustment of the hole depth will be easy. Reference product: Niigata Seiki drill stopper Order code: 86929525 Non-penetrating tapping threading is possible with this product's drill stopper matching the drill diameter. I would like to attach a stopper like the Niigata Seiki drill stopper (86929525) with one that was suitable for the drill size. Although the place of the shank is a hexagonal axis, the rear hexagonal shaft is easy to run out and the hole diameter may be larger than the drill blade diameter by about 0.3 mm, so I would like to stop the hexagonal shaft and make it a straight shank . "Runout error 0.3 mm is the allowable error range of the charging drill maker. By the way I am scraping off with a lathe in the case of a rear hexagonal axis. Then the vibration error becomes 0.05 mm or less.
This review is about item#35265316.
Plastic drilling
1
From Japan
On 2016-07-10 07:40:07
It is made for wood, but when used for plastics, the center shifts. The section is good. I feel I will not slip a little if the tip is sharp.
This review is about item#35265657.
Plastic drilling
5
From Japan
On 2015-08-19 22:37:07
Certainly it will cut cleanly. Plastics are sticky, so if you are told that burrs will come out, they are less, but they are less.
This review is about item#35265361.
2 mm thick aluminum drilling
5
From Japan
On 2015-06-19 15:01:47
Very beautiful hole and very easy to use. However, I have not done much work yet, so I'm a bit worried if the hexagonal axis and the drill part will not turn around at that time.
This review is about item#35265587.
To pilfer holes
5
From Japan
On 2014-11-23 06:29:17
As the product name, it was a good thing to cut quickly.
This review is about item#35265264.
Drilling of thin plates and soft iron materials
2
From Japan
On 2014-05-29 10:24:58
I think that it is a very good product with few clean burrs and a clean round hole for thin sheets and soft objects. However, there was also a fatal flaw. Hexagonal shafts are adopted mainly though it is supposed to be used with a hand drill, in particular the parts which are 6 mm or less are chucked separately and the knife part is press fit + It is bonded with adhesive. (It was so because it was scraped off with the grounder.) This is not very good. I bought various sizes, but the tip is all blurred. (It is not chuck or chucking blur but quickly the drill itself has blurring.) It may not be felt so much if it is a hand drill, but it is very well understood that it is blurred when used with a drilling machine. So it is often that the position shifts even if you punch firmly and start carefully. While it is a great tool, I felt it wastefully wastefully, so it is up to you to scrape off the hexagonal shank and remove it for this reason. Incidentally, things scraped off rotate without blurring, making it very easy to use. It is the same precision as the usual drill. So I wish I would sell an integral type of ordinary round shaft without having to bother with such a hexagonal shaft. There are things like a "plate paldrill" with a tip shape similar to Mitsubishi Materials, but this one has been sold for 10 sets, so if you order each size, you have to buy a lot in vain so It is unavoidable and can not be purchased.
Drilling of angle etc.
5
From Japan
On 2014-03-25 07:55:15
I like burrs less than the drills I used so far and I enjoyed very smooth hole making work.
We are using aluminum handrail for drilling work.
5
From Japan
On 2012-07-14 08:59:40
Since Bali is not so much, there is no necessity of deburring and I am very saved.
This review is about item#35265413.
Used for drilling of materials such as stainless steel, which takes time to remove burrs.
5
From Japan
On 2012-05-10 20:52:57
Since burrs do not appear, man-hours could be reduced. The hole shape is also close to a perfect circle. The material could also be processed similarly with stain, iron and aluminum. However, it seems that it is unsuitable for things with thick walls, round bars, etc. It broke during processing.
1
Customer Who Viewed This Item Also Viewed
Hexagon-head axis ironworking twist drill
Ultra Musashi drill
Drill Bit
DLC drill regular
DLC drill regular
Plate Pal Drill
Hex Shank Iron Drill
Hexagon-head axis puncturing