Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Cutting Bit, Bit Byte 3pcs

Cutting Bit, Bit Byte 3pcs
Sales Price: -
Review Rating: 4.67
3 Customer Reviews
5 star 2
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
Production of small parts
5
From Japan
On 2017-06-09 17:49:53
Both aluminum, brass and iron (S45C?) Are finished neatly.
This review is about item#35365793.
Manufacture of parts during lathe machining
5
From Japan
On 2016-08-08 16:32:00
I like it very much. With the grinder, because processing of the cutting edge can be processed freely
This review is about item#35365793.
As a part to make deburring of thin material
4
From Japan
On 2013-12-26 19:32:11
Although it is a wicked usage, I bought it as a material to make a tool called "deburring" of thin slicing (not for putting it on a cut-off holder and cutting it off). Although I do not know now, the old lathe has not made a special shaped bite that is not sold (it is not that difficult), but for work to remove the burr after scraping a thin thing, I also made a tool called "deburring" by burning material that was not baked in a fire and shaping it. So this is for cutting out, and the whole is baked (it is difficult to crack as it is dropped often if the whole is baked) but it is used to make deburr making by tapping red Although I thought, as I bought without investigating size or well, I was slightly too small to be impatient (I am bad) I welded a 3.2 mm steel plate and processed it to a normal length I think I will use it. (It is a little narrow, but I will endure it.) I think that people who use such a method are not even searching for the whole country, but for ordinary use, is not it good that they can be cheap with 3 pieces? If possible, I'd be happy to have data on width and length written in the item description. (Including other cutoff bytes (goods))
This review is about item#35365793.
1
Customer Who Viewed This Item Also Viewed
Solid tool
21 type (cut-off tool)
Completion tool bit, stick tool bit
Stick Bit Holder Set
Cutting Bit
Type 43 (cut-off tool)
Tool Blank
Parting Tool Holder
Solid tool
Parting blade holder
Parting blade
Plate tool
Cutting Bit Holder, Bit Holder