Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Programmable Relay Economy Type CPU Unit ZEN

Programmable Relay Economy Type CPU Unit ZEN
Sales Price: 139.99 SGD
Review Rating: 5.00
8 Customer Reviews
5 star 8
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Automatic control of drainage facilities
5
From Japan
On 2018-03-05 02:04:07
When using two or more timers and relays It is very handy to use this one because it is cheaper and usability is quite good. If the number of contacts for input and output are in time, you can do the same thing without using PLC
This review is about item#35502774.
Simplified sequence control
5
From Japan
On 2017-07-07 17:26:51
Usually this product is very satisfied to buy cheaply though discount is not useful. Reliability is also certain and ease of use is overwhelming compared to other products
This review is about item#35502774.
Automatic fish inducing machine
5
From Japan
On 2016-08-29 19:27:37
I am satisfied that I could form a circuit as my own circuit.
This review is about item#35502783.
Sequence control of self-made devices
5
From Japan
On 2015-09-03 22:50:47
Is ZEN special (original pricing is too cheap?), Almost no discount in direct sales. It is appreciated here because it can be obtained with special deals campaigns conveniently.
This review is about item#35502783.
Electric garage door opening and closing
5
From Japan
On 2014-08-06 16:53:32
Excellent cost performance. It is even better that the connection cable with the personal computer is a little cheaper. Even with manual input, there is no problem if it is a ladder diagram of about 30 lines.
This review is about item#35502783.
Valve control
5
From Japan
On 2013-10-23 08:50:59
It was used to set the time until the discharge valve was fully opened. Easily attached to existing equipment. By using the ladder program, there seems to be various uses.
This review is about item#35502774.
Control of flow control valve
5
From Japan
On 2013-07-29 11:13:41
It became possible to control to open the flow control valve over 30 minutes which we could not do so far. Depending on contrivance in the future it seems that there are also various uses. Although it was the first time for the ladder program, Omron's website has learning materials so I studied there.
This review is about item#35502774.
Automatic control of exhaust equipment
5
From Japan
On 2013-07-19 10:23:58
It was saved because we had quick response. It is "more than one thing to see" rather than explaining the operation by program.
This review is about item#35502774.
1
Customer Who Viewed This Item Also Viewed
Time Switch TB20K Series
Support Software ZEN
PC Connecting Cable ZEN
Micro Sequencer Fx3U Series, Basic Unit
Micro sequencer FX3G series (basic unit)
LED Type CPU Unit ZEN
Expansion I/O Units ZEN
CPU Unit ZEN
Battery Unit ZEN
SE01 series
Memory Cassette ZEN