Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Steel Made Drive Sprocket

Steel Made Drive Sprocket
Sales Price: 18.99 SGD
Review Rating: 4.71
7 Customer Reviews
5 star 6
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Maximum speed up
5
From Japan
On 2018-05-06 14:33:04
After changing to this, raiding around 40 - 50 km became quiet. On the other hand, the uphill will be a bit chaotic, but if it is up to 5-6% it will be fine.
This review is about item#35520353.
As a front sprocket of Super Cub 90
5
From Japan
On 2018-01-25 21:05:30
Cutting accuracy is good! I bought a cheap item before, but the accuracy was bad and I got a bit of noise and the drive chain immediately ran out of control.
This review is about item#35520353.
Exchange front sprocket on Cub 90
3
From Japan
On 2015-06-17 07:23:06
I was able to drive as I supposed.
This review is about item#35520362.
Used in Super Cub 90 DX 2002 formula
5
From Japan
On 2015-01-07 20:30:25
If you get accustomed to super cub genuine 15T and change it to 16T, will it start to run and acceleration is bad? I guess, I think that you can run unchanged as it is genuine by changing the timing of shift change. Feeling a pair of legs and two legs pulling more than genuine. Running around 60 kilometers the sound and vibration of the engine will be a little lighter, in my case, the fuel efficiency has also improved.
This review is about item#35520362.
Super Cub C 90
5
From Japan
On 2014-10-24 18:39:21
It was a perfectly good feeling with the chain change.
This review is about item#35520362.
Drive system renewal
5
From Japan
On 2014-01-19 20:30:43
I exchanged three points of the front and rear sproke and the chain of the Super Cub 110. Especially it is not a product that understands the difference, but I am very satisfied. It was exactly 10% OFF campaign, so 3014 yen in total! I have done a good shopping.
This review is about item#35520362.
I used it for Cub 90 custom.
5
From Japan
On 2011-07-17 03:10:41
Replacing the front 16T of Cub 90 reduces vibration and makes driving easier. Although it gets a little cheerful on a two-seater ride or a slope, it is worth changing.
This review is about item#35520362.
1
Customer Who Viewed This Item Also Viewed
Sprocket
Rear Sprocket
Drive Sprocket, Front
Sprocket
Rear Sprocket
Sprocket
Sprocket
AVAND- II cheek pad set
Drive sprocket
Brake Wire Cable