Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Drymet Lf, T0.5

Drymet Lf, T0.5
Sales Price: 0.99 SGD
Review Rating: 5.00
3 Customer Reviews
5 star 3
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
Motorcycle maintenance
5
From Japan
On 2015-10-16 18:25:48
I used it for a shift shaft of a motorcycle. It can be used for parts where there is no space for bearing installation. Since the main body is thin, we do not take up space. The operability is also good.
This review is about item#35511716.
Change of bearing of electric motor (domestic kitchen ventilation fan)
5
From Japan
On 2013-05-22 01:55:28
The rotation of the ventilator became heavy and it replaced. The bearing attached from the beginning was brass and 8φ length 10 mm extended to 9 φ and the hole was mounted on both inner surfaces of the case of the electric motor. Although it is a driving impression, it is quiet, smooth, and is a nice feeling. I used 5 mm for a 10 mm bushing, so I do not know the durability.
This review is about item#35511691.
Home bakery bread case repair
5
From Japan
On 2012-09-04 17:55:59
The bearings of the pan case of legal (the same as M KK) are abraded, resulting in the oil seal being broken. Although I was wondering if there is any other way to replace the breadcrumbs, I expanded the 10 mm bearings to 11 mm, but when I put this 0.5 mm thick dry meter up and down, there was no backlash and it revived spectacularly. Oil seal was also OK with 170 lbs of double lip bought here. In addition, if it is not 0.5 mm thick it will not enter up and down. And it is perfect to omit one washer below.
This review is about item#35511707.
1
Customer Who Viewed This Item Also Viewed
Drymet LF Washer
Drymet LF Bush
DDK05 Bushing with Brim
OILES #80 Bushing
DDK05 Bush
Gliteon F Bush
Collared Bush
Chip RCMT-14
OILES Flange Bush