Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Short bits for wood

Short bits for wood
Sales Price: 5.99 SGD
Review Rating: 3.40
10 Customer Reviews
5 star 3
4 star 3
3 star 1
2 star 1
1 star 2
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
For woodworking work
From Japan
On 2017-04-18 13:32:20
Currently used short bit has no top thread, but I think that it is easier to use this without it.
This review is about item#35595436.
During wood work
From Japan
On 2016-05-17 09:05:58
Because it can buy it cheaper than home center, it is saved. Sharpness is no problem.
This review is about item#35595454.
Wood drilling work
From Japan
On 2015-12-11 11:13:40
We opened the package and confirmed the cutting edge first, polished on the outside, but we did not know what was caused by polishing inside, but the burr did not become a large blade. We decided to polish the back of the blade here and use it. Firstly, inspection after production is not done! Please make sure you have good products.
This review is about item#35595402.
Drilling φ21 into the door of the tree for the final locking
From Japan
On 2015-11-14 14:02:31
Sharpness was bad and I took time. However, because it is one time use, it helped enough. If you have multiple holes, we recommend you to buy better things.
This review is about item#35595533.
From Japan
On 2015-10-05 13:51:42
Normal upper class !!
This review is about item#35595454.
From Japan
On 2015-03-13 17:10:37
You can drill beautiful holes at high speed with impact. The speed of drilling is surprisingly fast, working efficiency is high.
This review is about item#35595533.
From Japan
On 2014-12-19 12:19:15
Although I bought it from a cheapest one, I bought it from a cheapest one, but it is bad, it has burrs on its surface, it is a high level job, so it will not be used. The price is cheaper than the first-class maker, but because it did not become usable, it became high shopping.
Drill a hole to pass one wire through electric wiring
From Japan
On 2014-06-27 19:19:25
This purchase is also a repeat. It's quite good !!
This review is about item#35595506.
Processing of parts
From Japan
On 2013-08-09 13:19:55
Although it is not cheapest, it is the bit that can be most reliable in using it.
This review is about item#35595384.
Pilot hole for woodworking tapping screws
From Japan
On 2013-08-07 19:11:09
I bought two, but one of them is not in the center, it is in a state of turning around when turning it by turning it on a drill board. The other one is usable normally. Depending on the characteristics of the product, it often goes into the tree, so if you use it with a rechargeable electric drill, the hole strikes deeply. I think that this is a usage problem, but it is a bit hard to use as a way of using it.
This review is about item#35595384.
Customer Who Viewed This Item Also Viewed
Super Woodworking Drill
No.1 short bits
Forstner Bit
No. 2 combined use bits
No. 6 multiuse bit
Woodworking stopper bit short
Brad Point Bit
No. 5 short bit
Short Bits For Wood
Combined Bit