Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Rod End, Lubricated Male ThreadLeft Screw Type

Rod End, Lubricated Male ThreadLeft Screw Type
Sales Price: 7.99 SGD
Review Rating: 3.86
7 Customer Reviews
5 star 2
4 star 2
3 star 3
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
At the rod end
5
From Japan
On 2016-07-19 06:21:02
It is cheap and saved. Lifespan is unknown as it is about tomorrow.
This review is about item#35727605.
Car toe control arm pillow ball support
5
From Japan
On 2016-01-28 14:10:33
It was cheap and used by replacing the same thing made by another company. Piro's movement was tight, the thing with the highest precision without any play was arrived, I was satisfied very much! It was the highest precision component that was unlikely to be possible from the price and was the best member with no play. If the same accuracy as the left screw you purchased will come out at the same price in the future, I would like to continue to use it. I hope that it is best if there is a right screw made at the same place as the left screw that I purchased, if possible. This series, the static load is also higher than other companies' products before the exchange, and it is Osaka soul close to the no-brand, but it seems that performance which can not be reckoned is contained. However, there was a variation in accuracy that I thought whether there was a disappointment, right and left had variations in accuracy. The left screw which seems to be hit was super bargain because it was God precision which can not be at this amount of money.
This review is about item#35727641.
Used in ATV
4
From Japan
On 2014-12-02 09:14:14
Used as a handle tie rod end However, the screw pitch did not match and it was necessary to replace each rod.
This review is about item#35727614.
Used for motor related parts
3
From Japan
On 2014-05-25 16:48:23
Although the price is satisfactory, is grease bad, there is a spot, there is dirt (improvement point)
This review is about item#35727605.
Car suspension
4
From Japan
On 2012-04-05 17:29:59
Although it is cheap, it can be used without problems. I want a long rod.
This review is about item#35727657.
Machine parts. Motorcycle parts.
3
From Japan
On 2012-03-22 12:41:35
The goods themselves have a feeling of use especially unlikely and unavoidable rod end. The right-handed screwdriver type with 8 mm and 10 mm pairs is not the Osaka soul brand but the MonotaRO brand, and the manufacturer of the goods delivered is also different. If you use it separately, rabbits also use horns, left-handed screws with right-handed screw type When pairing with manufacturers saying somewhat disturbing. Although it is an overseas manufacturer item, it can not be felt that the price is less expensive than the domestic manufacturer's item. Considering the possibility that manufacturers change every time, I think that we will avoid purchasing next time.
This review is about item#35727605.
Universal
3
From Japan
On 2012-01-23 16:37:44
It is as innocent as a famous manufacturer.
This review is about item#35727596.
1