Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Thin-Shaped Magnetic Catch

Thin-Shaped Magnetic Catch
Sales Price: 2.99 SGD
Review Rating: 4.20
5 Customer Reviews
5 star 3
4 star 1
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Installation of signboard for event
5
From Japan
On 2017-03-15 14:14:51
I used it for the event signboard on the condition that it can be securely attached and easily detachable. It was thin and compact, but the magnetic force was strong, so it was able to fulfill the purpose.
This review is about item#35758441.
For installation of BOX etc.
5
From Japan
On 2014-12-10 10:33:31
In the item explanation, "※ Please use M2.6 Sarah Small Screw or Sarah rivet for installation", but you can go with M3 Sarah Small screw without problems.
This review is about item#35758441.
To fix the door when opening the self-closing sliding door.
5
From Japan
On 2014-11-10 07:54:24
Both shape and magnetic force were good.
This review is about item#35758441.
Installation of tool
2
From Japan
On 2014-10-02 15:41:54
Surprisingly the magnetic force was good
This review is about item#35758441.
It is used as a magnet catch to fix the opening / closing part.
4
From Japan
On 2013-06-28 13:56:25
It is difficult to use that the strength as a magnet is unevenly distributed around the periphery. While thinking that it is inevitable as a magnet, it is easier to use if there is maximum strength in the center. Since only the magnet part protrudes from the mounting part in a circle, it is difficult to remove the mounting position. Easier to use if it is rectangular including the mounting part. I am satisfied with the magnetic strength.
This review is about item#35758441.
1
Customer Who Viewed This Item Also Viewed
Dust Proof Magnet Catch
Magnetic Catch
Flat Magnetic Catches
Thin-Shaped Magnetic Catch
Thin Magnetic Catch
Magnetic Catch
Magnet Holder
Magnetic Catches
Magnetic Catches
Magnetic Catch
Magnetic Catch