Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Resin Bearing DR-H, Standard Type) TYPE4

Resin Bearing DR-H, Standard Type) TYPE4
Sales Price: 1.99 SGD
Review Rating: 5.00
4 Customer Reviews
5 star 4
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
During wood work
5
From Japan
On 2016-08-14 22:27:59
I am very satisfied with the function.
This review is about item#7273436.
Replacement of rollers at the lower end of foldable shutters
5
From Japan
On 2016-01-20 16:05:24
Replacement parts could not be obtained due to discontinuation of production, but I found a roller of almost the same size on Mr. Monotalore's HP. It made it possible to open and close the shutter smoothly and also thank you very much for the reasonable price.
This review is about item#07273497.
Door roller of storm door
5
From Japan
On 2015-10-22 15:59:40
I was glad to see it but it was very good if there were ones with W1 and W2 1 mm.
This review is about item#07273454.
For conveyor movement
5
From Japan
On 2015-08-05 00:58:25
Used as a foot for moving a lightweight conveyor. It is very smooth. The resin part is hard. Also, although the rugged sound is big, it is probably because the resin is hard. This product can be recommended if load capacity and volume allow.
This review is about item#07273506.
1