Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of 18-8 Measuring

18-8 Measuring
Sales Price: 8.99 SGD
Review Rating: 4.71
7 Customer Reviews
5 star 5
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Weighing of materials
From Japan
On 2017-11-23 09:06:50
I think that it is a quality commensurate with the price. There is nothing dissatisfied in particular.
This review is about item#35789941.
Melt the gel
From Japan
On 2015-03-04 15:06:30
I bought a thing with a capacity of 1L and 0.5L. Both had the thickness of stainless steel, the making was solid. You can dissolve candle gel and work well. It seems to be good if there is burn injury prevention, such as sowing a ribbon on the hand part.
This review is about item#35789914.
When mixing
From Japan
On 2015-02-19 14:38:40
It is easy to use.
This review is about item#35789941.
Pour gasoline into a small engine machine
From Japan
On 2013-09-25 13:20:21
Pouring into the gasoline tank with a handy kerosene pump, I purchased it because there may be overflowing occasions. It is a measuring cup with a mouth, so you can pour it without spilling and I am very satisfied. Until now I was poured with a plastic measuring cup, but because it melts against gasoline as a material, it is saved if it is stainless steel.
This review is about item#35789914.
Weighing of solution
From Japan
On 2013-09-09 21:02:46
I got the impression that it is solid even at low price.
This review is about item#35789923.
For Outdoor
From Japan
On 2013-09-03 13:51:31
Make it solid and withstand rough use outdoors.
This review is about item#35789941.
Liquid pesticide measurement with large sprayer
From Japan
On 2013-08-09 13:36:12
Notice rust with SUS 304. Even though it is inexpensive. The balance of the handle is good, easy to pour with a mouth! (^ Ω ^) We can not measure less than 500 cc, but when pesticide to be thrown into a 1000 liter tank of sprayers is about 3.5 liters. Resin made of 1 to 2 liters of capacity is not user-friendly and does not have durability, so stainless steel objects that can withstand chemicals are the best.
This review is about item#35789957.
Customer Who Viewed This Item Also Viewed
Stainless Steel Beaker
Beaker Stainless Steel 18-8, SUS304Handleless
18-8 Beaker
Handle Beaker Lid
18-0 Darker
Thick Beaker Mugs
18-8 measuring cup
Measuring Cup
Bath chair S25