Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Standard V Pulley M Type

Standard V Pulley M Type
Sales Price: 7.99 SGD
Review Rating: 4.57
7 Customer Reviews
5 star 5
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Machine modification
5
From Japan
On 2016-02-29 15:49:58
An amateur is not a product that can easily pierce with a drilling machine, but if you have a lathe, grasp the shaft part, turn the pulley, bring the fixed drill close, and open it in the center as you drill a hole. It is well-balanced with the manufacturer's products and can be drilled freely according to the shaft diameter so that it can be used for anything. For amateurs, is it better if you can specify the size of the hole and have a service to open it?
This review is about item#36168081.
Motorbike remodeling
3
From Japan
On 2015-11-19 19:43:07
Drilling is difficult because the center has not come out.
This review is about item#36168027.
Connecting the power side of the generator to the generator
4
From Japan
On 2015-08-31 15:23:23
It is used when transmitting the axis of the windmill on the vertical axis to the generator, it is originally intended to convey the power of the engine, but it is thick and heavy, it is not suitable for wind-powered hydroelectric power generation, on a lathe We cut down the meat and made the weight light, but there was not much merit. It will be purchased when transferring power to large generators in the future.
This review is about item#36167993.
Power transmission of mini machine tool
5
From Japan
On 2015-05-17 20:46:25
It is very usable. I think the cost performance is quite good.
This review is about item#36167993.
power
5
From Japan
On 2015-02-12 09:55:27
Since it is a maker item, it was able to be used without problems.
This review is about item#36168011.
Machine tool creation
5
From Japan
On 2014-04-28 16:41:14
good
This review is about item#36167993.
Repair of the drilling machine
5
From Japan
On 2013-02-17 15:00:30
If there is a punch marking in the center of the pulley, even an amateur can be processed without blurring.
This review is about item#36167993.
1
Customer Who Viewed This Item Also Viewed
Standard V Pulley Atype
SP Pulley
Standard V-Belt Pulley A-2
Jis V-Belt Pulley A-1
Standard V-Belt Pulley A-1
Standard V-Belt Pulley B-1
SP Pulley
V-Belt Pulley A-2
ISOMEC SP Pulley SPA-1
NS standard V pulley B-1
Wedge pulley 3V form
ISOMEC SP Pulley