Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Metal Protest Formula Pipe Coupler Connector

Metal Protest Formula Pipe Coupler Connector
Sales Price: 3.99 SGD
Review Rating: 4.71
7 Customer Reviews
5 star 5
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
It is used as a pressure guide pipe of water pressure measurement equipment.
4
From Japan
On 2018-03-07 15:22:16
It is saved if you clearly specify the setting of the tightening torque value of biting ring, it is tightening at present.
This review is about item#37102545.
Air piping for driving the steam valve
5
From Japan
On 2017-08-31 15:34:02
Price, good quality. It is more expensive than the pipe material store, but it is a great place for monotail to get all these things.
This review is about item#37102502.
Clamp removal during machining
5
From Japan
On 2017-05-30 16:43:07
It was able to be used without problems. It will be appreciated as it arrives quickly, the length can also be made freely in combination with the copper pipe.
This review is about item#37102624.
Plumbing for kerosene
4
From Japan
On 2017-03-02 20:38:43
It was cheap, very easy to use, and worked smoothly.
This review is about item#37102642.
Installing water heater
5
From Japan
On 2016-04-27 01:16:54
It was good to be able to connect directly to the 15 mm piping cheese
This review is about item#37102642.
kerosene
5
From Japan
On 2016-01-16 18:32:07
There is no problem.
This review is about item#37102527.
For oil supply piping
5
From Japan
On 2015-02-20 15:03:23
I am satisfied with the parts as desired.
This review is about item#37102642.
1
Customer Who Viewed This Item Also Viewed
Ring Joint Screw
Connector
Smoothing copper tubes
Male Adapter
Joint for Copper Pipe
Ring Ball
Flare Joint
Ring Elbow
Ring Joint
Union Elbow
Union Tee
Union Connector