Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Wire Cut

Wire Cut
Sales Price: 3.99 SGD
Review Rating: 4.12
8 Customer Reviews
5 star 3
4 star 3
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Factory partitions
4
From Japan
On 2018-04-27 15:04:44
It is quite thin and easy to handle. The price was reasonable and good.
This review is about item#58926253.
Hanging the frame
3
From Japan
On 2017-12-06 14:22:32
Because I am not satisfied with just receiving forehead. I can use it without problems.
This review is about item#58926217.
As a fall prevention code of waist tool
5
From Japan
On 2017-01-12 22:58:45
I think that you can work even in a very wide work area if you connect a tool with a long cable of a strap and connect with a wire with this wire. Also the load capacity is very high, it is very satisfying because it was very cheap. I will repeat.
This review is about item#58926235.
Muffler cutter drop off prevention
5
From Japan
On 2016-09-29 21:59:11
The length is just right The diameter of the eye part should be slightly larger.
This review is about item#58926235.
To reinforce the ceiling hanging speaker
4
From Japan
On 2016-07-15 11:42:01
It has been processed at both ends, but it is good if there is a product line-up such as 4-piece set, etc., with one-sided eye processing, suppressed the price a little more.
This review is about item#58926271.
Wire winding over prevention device in track lane
4
From Japan
On 2014-12-11 14:34:18
Terminal processing is clean. The price is also cheap.
This review is about item#37137152.
To prevent the fall of the TV during the earthquake
5
From Japan
On 2014-07-15 13:55:02
I stretch two left and right on the back of the TV and heat it to the TV stand and use it. With one load capacity: 20 kg, so there is no problem with strength. It is polite to make it for the price.
This review is about item#37137292.
Outboard engine parts
3
From Japan
On 2014-05-14 23:18:28
Although it is a good feeling of use, there is a problem with strength
This review is about item#37137116.
1
Customer Who Viewed This Item Also Viewed
Stainless Steel Wire Rope
Wire Rope
W Sling A Type Wire
Wire Rope Slings
Oval Sleeve
Satsuma Lock Slinging Wire
Out Stand Wire Winding Flemish
Stainless Steel Wire Rope (SUS304)
Wire Key Ring
Color Boots AZ-4706