Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of FB Super Fine Belt

FB Super Fine Belt
Sales Price: 42.99 SGD
Review Rating: 3.50
6 Customer Reviews
5 star 1
4 star 3
3 star 0
2 star 2
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Polishing of metals, woodworking products
4
From Japan
On 2016-12-03 19:29:18
It is better to sell one. Since it usually sells 10 sheets, it is enough for a small amount when used for hobbies such as DIY. Also, I am afraid that it is a unit of ten sheets of belts that I do not know whether it is good or not, and I can not get a hand at a high price. I would also like other belts to consider selling one sheet by all means.
This review is about item#37302352.
Modified polishing of stainless steel HL material
4
From Japan
On 2015-09-17 16:57:15
# 60 is used but since stainless steel is hard it does not count its eyes as it gets numbered (it is finer than the # 180 of the HL material of the manufacturer's polished) so that a harder abrasive can be used even with stainless steel using a harder abrasive want
This review is about item#37302404.
Copper, copper alloy hairline and scratches and oxide film dropping.
2
From Japan
On 2015-06-20 00:33:10
I bought this product of 600 number which 3M goods only had up to 400 and the price was a bit cheap, but it is easy to pierce anyhow! Especially at both ends, it is noticeable, but if you hit a workpiece (especially if you hit the edge of the workpiece) it will be peeled. Is it the only advantage that it is easy for familiarity to work with thickness and curved surface? I want to raise durability.
This review is about item#37302413.
Polishing of cutlery
2
From Japan
On 2014-06-30 13:54:40
Too much thickness
This review is about item#37302352.
Woodworking
4
From Japan
On 2013-08-21 22:01:34
Used for general woodworking work, purchase all counts. A series of polishing sensations. Good goods with it.
This review is about item#37302404.
Final polishing
5
From Japan
On 2013-08-05 06:38:52
The thickness is really good. I could not use normal 1000 number purchased at the same time, so I would like to continue using this one.
This review is about item#37302352.
1
Customer Who Viewed This Item Also Viewed
Zirconia Endless Belt
Scotch-Brite finishing belt
Endless belt
Zirconia Belt
Endless belt (No. 36 A belt)
FB Abrasive Belt
Zirconia abrasive belt (ZRHUZ)
Finishing Belt
217EA Tri Zakuto belt
Endless Belt, EBB
Panda sandals
Unilon Belt
Ricoaz Belt