Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Magnet Bit Holder

Magnet Bit Holder
Sales Price: 12.99 SGD
Review Rating: 5.00
5 Customer Reviews
5 star 5
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Electric installation · Air conditioning construction in general
5
From Japan
On 2014-11-03 03:12:25
In the same type of magnets, I think that the strongest magnetic force is good. Once you start using it, you feel it is hard to do without it. I think that dissatisfaction points also have compatibility with the bit, but because you may get this self you will not fall, we use vinyl tape wrapped around it. It was disappointing that we could not use it as a bit of the torsion type, so we lost it a lot. It is awesome if this neighborhood is resolved. Also, the price is a bit high. I feel that I can do it a little more cheaply but how do you feel?
Electrical wiring work
5
From Japan
On 2014-03-10 04:35:08
The magnetic force of the magnet is also strongly satisfied. It is even better if there are more kinds of colors.
This review is about item#37150924.
DIY's help
5
From Japan
On 2013-09-16 06:48:52
It can be used for most bits and is convenient. It is useful if there is fluorescent dye in the main body
This review is about item#37150924.
Remove screws in a narrow place
5
From Japan
On 2013-04-24 09:15:58
Very satisfied
This review is about item#37150924.
Sheet metal work
5
From Japan
On 2013-02-13 14:12:45
The adsorption power of the magnet is also strongly satisfied than I thought
This review is about item#37150924.
1
Customer Who Viewed This Item Also Viewed
Mug Fit
Mag Dry Power, Dry Bar Magnetizer
Magnetic Catch
Magnetic Screw Catcher
Magnetic Screw-Holder
Magnetic Screw Catch
Magnetizing Holder
Magnet Bit Holder
Magnetic Catch
Magnetic Catch
Screwdriver Magnetizer Demagnetizer
Magpita
  • Magpita
  • SUNFLAG (SHINKI MFG)
  • 4.99 SGD
SF Pitattokun
Magnetic Catch
Ultrashort mug catch