Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Mug Fit

Mug Fit
Sales Price: 19.99 SGD
Review Rating: 2.33
3 Customer Reviews
5 star 0
4 star 1
3 star 0
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
From Japan
On 2015-07-10 17:05:03
I used several hundred yen similar products (not falling), but I bought it with expectation because it is a high price item. Unfortunately the magnetic force was weak and it was disappointing.
electric screwdriver
From Japan
On 2014-04-16 20:17:27
When two are attached, the magnetism becomes weak. I tried both sides but it was no use. I think that the magnetism is weak a bit with one piece and want me to tell me how to use 2 pieces if I can. Currently I have patience with using 1 piece.
This review is about item#37018737.
Used for thin shaft bit
From Japan
On 2013-07-09 18:24:38
Although it is used to hold the no-op race, it can be held as it is if attached to the bit tip, but since it is inevitable because it is inevitable, it is lowered to the rear of the bit and it is used. If you lower it to the rear, 100 mm bit does not know the feeling of use · · · 65 mm bit is not even better than just nothing. I want the magnetic force three times more, are there no thin shaft magnets at other companies? It seems like I do not use it. In this case we will not purchase it even at a list price of \ 200.
This review is about item#37150942.
Customer Who Viewed This Item Also Viewed
Magnet Bit Holder
Mag Dry Power, Dry Bar Magnetizer
Magnetic Screw Catcher
Magnetic Catch
Magnetic Screw-Holder
Magnetic Screw Catch
Magnetizing Holder
Magnet Bit Holder
SF Pitattokun
Ultrashort mug catch
  • Magpita
  • 4.99 SGD
Screwdriver Magnetizer Demagnetizer