Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Metal Joint

Metal Joint
Sales Price: 5.99 SGD
Review Rating: 4.17
6 Customer Reviews
5 star 3
4 star 2
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Work supporter
5
From Japan
On 2018-02-05 08:03:15
We can use it as a thing indispensable for building a table according to space and use.
This review is about item#37168467.
Creating a three-stage pipe bed
4
From Japan
On 2017-12-25 22:33:35
The two-stage pipe bed is overflowing in the streets cheaply but it becomes difficult at once because it becomes three stages, so if you make it yourself, buy it, truly when you reach 3 stages the upper stage will shake even in metal joints, the number of pipes and braces etc. I thought that it was necessary to devise some additional purchase so it seems to be additional purchase.
This review is about item#37168634.
Pipe rack production
5
From Japan
On 2017-11-14 16:45:45
Arranged, I was able to complete the production at the scheduled schedule by shipping the next day
This review is about item#37168634.
When using the ejector, because it is weak in the plastic joint member, it is used for reinforcement
5
From Japan
On 2017-04-27 15:22:49
The joint is crucial Place elbow is a good fitting to amplify the degree of perfection by using this as it is expensive as danger remains afterwards.
This review is about item#37168467.
Light truck bed shelf installation
2
From Japan
On 2015-04-16 23:31:25
Because dimensions such as Φ were not clear, I was very lost.
This review is about item#37168512.
Personal computer monitor stand etc.
4
From Japan
On 2014-07-15 14:04:33
It is used for fixing the monitor stand and the speaker of the personal computer. Building a building of 350 mm from the top of a commercial PC desk, we designed it to jump 400 mm horizontally from there and used it for this intersection. The monitor was 4.8 kg, the speaker was about 2.2 kg, but although it was slightly shaken and attached with grafting, it could be fixed to the extent that it is practically unnecessary. Also, unlike plastic joints, positioning is easy since it can be adjusted by slightly loosening the bolts even after all assembling. I am sorry if the price is a bit cheaper. . .
This review is about item#37168512.
1
Customer Who Viewed This Item Also Viewed
Standard Pipe,
Plastic Joint
GA-1S set goods
GA-2S set goods
GA-7S set goods
Elector metal joint
Plastic joint
Twist 45 rat pants 2143
Metal Jiyo points
Metal Pipe Joint
Adjuster
Elector phi28 pipe