Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Double Ring

Double Ring
Sales Price: 9.99 SGD
Review Rating: 4.50
4 Customer Reviews
5 star 3
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
When hanging display version, use with ball chain.
3
From Japan
On 2018-01-11 15:29:30
Every month, regularly sell with display version with ball chain, connector and To use it, it is good to be able to order in batches.
This review is about item#37181094.
Used when lower leg locker key is exchanged
5
From Japan
On 2015-12-12 15:21:57
I am firm and have a sense of security.
This review is about item#37181094.
I use it for binding of document of about 10 ~ 30 pages such as a procedure manual to be handed over to students at PC classroom.
5
From Japan
On 2015-09-24 09:51:59
Because ring binding can be folded into two with the desired page as a table, it takes only one sheet of paper at the desk. Two to four holes are punched in 2 holes. The wearing of the ring knows that the wooden bar of the ice bar is very strong, scrape one end with a cutter into a tongue and make a jig with a notch so that the wire of the ring fits about 10 mm from the tip It was easy to install. The ring diameter, the cross section of the strand (○ type), the strand thickness, the material, the quantity of one pack, the brand name was Nomark which chose this product. Since the shipping cost was about the same as the price of the item, the unit price of the ring became about ¥ 5, and it became ¥ 20 per document. If there is a ring of the same size, I thought that I would like to seek in the nearby home center from the next time.
This review is about item#37181085.
To connect the case and the case
5
From Japan
On 2015-04-02 16:40:34
Previously, I used a thing with double price, but changed to here half price, usability was also unchanged. I am very satisfied.
This review is about item#37181094.
1
Customer Who Viewed This Item Also Viewed
Keyring
Double Ring in Plastic Case
Key Ring, Steel
Stainless Steel O-Rings
Double Ring
Double Link, Stainless Steel
Double Coil
Split Rings
Chrome double ring
W Ring, Double Ring
Nickel W Ring