Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Couplicon MRG Series

Couplicon MRG Series
Sales Price: 9.99 SGD
Review Rating: 4.67
6 Customer Reviews
5 star 4
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Used as a joint for DC motor
4
From Japan
On 2017-05-10 16:38:35
Parts that are perfect for functional aspects and materials. However, is there anything we can do for minor scratches on the surface? I already use it, but it is functional enough. For price, it is good if it is cheaper a little, but I am satisfied with the use.
This review is about item#37531426.
Machine tooling, prototype
4
From Japan
On 2017-01-16 11:52:46
Production accuracy is good. Because it is used for the rotary shaft, it is desirable for the application to be a little more tight.
This review is about item#37531523.
Used to connect 3 mm motor shaft and drive shaft
5
From Japan
On 2015-11-24 17:33:47
The hole to insert the 3 mm motor shaft was a bit irritable but I managed to get through. Since the person of 6 mm was a stringer bolt, it originally entered a small diameter without any problem. I would appreciate it if you have dimensional tolerances in the inner diameter of the specification column. In the 6 mm hole, the tapping screw was cut in two places, I thought that the detail was taken into consideration. Although I have not actually used it yet, it is good with feeling of operation confirmation.
This review is about item#37531444.
Motor and driver connection
5
From Japan
On 2015-05-29 16:23:23
If you have a good opportunity for accuracy, I'm thinking of buying again
This review is about item#37531435.
Stepping motor bearings
5
From Japan
On 2015-03-25 13:59:30
The shaft of the stepping motor was φ 5 mm, and the target shaft to be driven was φ 3 mm, which caused trouble in connecting. There are such parts. Moreover, it is attached to the shaft fixed anion screw. We satisfy our request 100%. it is perfect.
This review is about item#37531435.
In order to convert variable resistor of inch dimension axis to common shaft diameter
5
From Japan
On 2015-02-13 00:44:41
By fitting the sleeve on the inch dimension axis it will be exactly 8 mm, so this different diameter joint could be used. Despite the necessity of depth, the general dial knob can not be used because the variable resistor is special. Since the dial for the inch shaft is custom-made, it was within the range that can be convinced when considering the overall cost.
This review is about item#37531523.
1
Customer Who Viewed This Item Also Viewed
Couplicon Mini Set Screw Type
SPR FLEX Coupling
Soft Flexible Coupling Couplicon MSF Series
Couplicon Mini Set Screw Type
Couplicon Mini Set Screw Type
Rigid coupling AR , ARC series
Capricone MLR series
Flexible Coupling
Rigid coupling RAS type
Rigid coupling RSS type
Motor Coupling 16 x 10
Motor coupling 16x6
Motor Coupling 19 x 10