Buy more than* S$200* and get FREE SHIPPING
Due to the national holidays as Golden Week, we will close 2018/4/28~2018/4/30 and 2018/5/3~2018/5/6.
This may cause delays with our responses. Thank you for your understanding.

Customer Reviews of Nylon Tube, Black, 5M

Nylon Tube, Black, 5M
Sales Price: 4.99 SGD
Review Rating: 4.77
13 Customer Reviews
5 star 11
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 13 of 13 Reviews
Purchased to spare.
5
From Japan
On 2017-10-15 11:04:59
Purchase because air leakage will occur because order code: 07320783 and order code: 87896356 are incompatible. The compatibility between the manufacturers is still better.
This review is about item#37563163.
In the work work
5
From Japan
On 2017-03-30 10:27:25
If you look at some of the machines' exhibits and make your own from too expensive, you can inexpensively have higher performance than that.
This review is about item#37563172.
As an air hose of a large truck.
4
From Japan
On 2017-03-24 09:13:19
It was nice to have this size because it was quite unusual. The goods themselves can be locked tightly and can be used without causing air leakage. I wish it had more variations of size because it did not enter so long this time.
This review is about item#37563206.
DIY. Making a gimmick for fishing gear
5
From Japan
On 2016-09-30 17:14:54
The item description was easy to understand and the item as per the image arrived and I felt happy.
This review is about item#37563154.
Used during painting work
5
From Japan
On 2016-09-30 16:16:34
I bought it to add a filter and a regulator to the compressor.
This review is about item#37563181.
Compressed air piping
5
From Japan
On 2016-08-08 21:12:54
It is very helpful because there are not 8 mm tubes inside.
This review is about item#37563172.
Repair parts of tire changer
5
From Japan
On 2016-05-11 13:08:44
There is no problem with accuracy!
This review is about item#37563172.
Cleaning water piping
3
From Japan
On 2015-08-18 15:57:34
It is easy to drill hole by drilling, it is suitable for one-touch fitting with moderate hardness and is easy to use. I think that it is still better if you can purchase from the minimum unit of about 3 m.
This review is about item#37563197.
Used for air suspension.
5
From Japan
On 2015-01-15 13:22:10
When ordering a nylon tube separately (3.000 yen or less), since the shipping fee is added, it is appreciated if you can ship by e-mail facilities.
This review is about item#37563172.
For instrumentation equipment operation air supply
5
From Japan
On 2014-09-06 09:26:45
Because it is rarely used diameter, it is good to be able to purchase in short units.
This review is about item#37563181.
Compressed air equipment
5
From Japan
On 2014-05-26 13:27:54
good
This review is about item#37563172.
It is used for pressurization test
5
From Japan
On 2014-01-30 15:03:59
It can be used without problems. I would like to purchase from here as well next time.
This review is about item#37563163.
It connects to an air cylinder.
5
From Japan
On 2013-09-06 20:57:00
The feeling I used is very good.
This review is about item#37563181.
1
Customer Who Viewed This Item Also Viewed
N2 Series 5 M White Nylon Tube
Polyurethane Tube Black
Nylon Tube N2 Series 5 M Blue
Tube Fitting Elbow
Soft Nylon Tube Black
N2 Nylon Tubing
Nylon Tube White 5m
Nylon Tubing