Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Parallel Pin, Stainless SteelA Type M6, Plus Tolerance

Parallel Pin, Stainless SteelA Type M6, Plus Tolerance
Sales Price: 13.99 SGD
Review Rating: 3.50
2 Customer Reviews
5 star 0
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 2 of 2 Reviews
To prevent idling of rotating parts
4
From Japan
On 2013-09-14 17:52:59
Although it is a 25 mm long standard, we measured a few, but it is only 2.49 mm - 2.48 mm in actual measurement. Although this rank may be in the range of error, it is bad feeling for short, so I do not know whether to purchase next time.
This review is about item#37571904.
It is mounted by a certain maker made for the impeller (impeller) of the discharge pump and it is mounted as it is for replacement if there is damage of the pin every maintenance. When purchasing from the manufacturer it takes time to deliver and it may not be able to respond to a sudden job, and if you order the price quite considerably
3
From Japan
On 2011-12-16 14:31:43
Actually I wanted a length of 15 mm, but since it was not made as a product, I ordered 18 mm this time. I was wondering if I could substitute at 18 mm, but I was wrong. Since I bought it with great care, I cut it for a long time with a file and use it. I think that there is no problem as a product. I hope there is 15 mm. When purchasing from the manufacturer, it takes a long time to deliver, not to mention a high price, so it may not be possible to respond suddenly. I ordered this time. Hattaro is quickly delivered, and its price is cheap.
This review is about item#37571877.
1