Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Double Legged Stand With Auto Lock Mechanism

Double Legged Stand With Auto Lock Mechanism
Sales Price: -
Review Rating: 3.91
11 Customer Reviews
5 star 7
4 star 1
3 star 0
2 star 1
1 star 2
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
At the time of bicycle stand
4
From Japan
On 2014-06-20 11:20:16
It is okay if there is stability feeling Plating part rusts
This review is about item#37586771.
Very light
5
From Japan
On 2014-04-10 15:37:56
I purchased it for women's bicycle. It gets very light. Even with heavy luggage being loaded, perhaps it is a momentum to rise even with children. It will lock when you stand up. It is also hard to fall down because it has a good sense of stability. It was a good item I had bought earlier.
This review is about item#37586771.
As a 24-inch electrically assisted bicycle repair part
1
From Japan
On 2013-11-02 20:14:14
I bought it for 24-inch as a replacement part of a 24-inch electric assisted bicycle (Honda Racoon). WO24 × 1-1 / 2 attached to the tire installation car where it interfere with the tire and it was impossible to install. Since the chain was also stretched, it was exchanged and adjusted to relax the chain tension, it was able to install because the gap was empty as much as 2 mm, but since there is no adjustment fee when the chain stretches, it is not likely to be used actually . I should have used it for 26 inch. It is a non-refundable item so it has become useless shopping.
This review is about item#37586753.
I will carry your luggage
5
From Japan
On 2013-10-26 21:04:54
A stand excellent in stability excellent in cost performance was able to be worth the price with Monotaro san.
This review is about item#37586762.
Attached to a body with weight such as electric assisted cars.
5
From Japan
On 2012-08-01 18:49:14
very good. It seems that it is special surface processing, but everyone who sees me asks "I am stainless steel?" It is okay to lock it automatically, just stepping on the step part to fix it, it is excellent to be able to make a heavy body easier. It is wide and strong against crosswinds. As a general recognition (of a bicycle shop), this type of "compatible stand" can not be mounted on a bicycle with external transmission. There is also a dedicated thing, but it is not durable. Therefore it is natural that this product is not attached. It is now one of the few domestic parts manufacturers.
This review is about item#37586762.
I used it for 6 months
5
From Japan
On 2012-06-12 13:46:37
Used in a half year rain. Unlike the cheap stands, when the oil runs out and rust develops, the stand does not easily rise. It is a feeling that it finally goes up after hitting the killer. When you pour 100 yen bicycle oil, it revives beautifully. It becomes a smooth movement at the time of purchase. It is a product with clear lubricant effect.
This review is about item#37586771.
Since the age of the user is 80 years, it is easy to raise it and it is selected as a thing hard to collapse
5
From Japan
On 2012-05-14 16:12:48
Because it is a motor-assisted bicycle, it was a point that it is not necessary to lift as it is an electric assisted bicycle It is easy to step on just as you step on and a lock is also batched. A lock release is also easy. Because it is an old man of 80 years old, it was hard to lift the car body to hang the stand I think that it is a very excellent structure Also it does not feel like collapsing even if you ride with the stand hung, it is very different from the standard stand which was very stable Incidentally, it is Panasonic's Vivi · NX 24 It is inch (interior 3 steps)
This review is about item#37586753.
Stability enhancement to put the child behind
2
From Japan
On 2012-04-10 20:49:18
I would like you to clarify that you can not install on exterior gear cars. Because it is impossible to return it, cut it with a grinder and weld it at an iron workshop near the existing stand and cope with it. Thanks to that, I was sorry that it was expensive. Because we have good products, the lack of information is very disappointing.
This review is about item#37586771.
Repair application
5
From Japan
On 2012-04-02 00:48:03
Even though we compare it with owned BS, even if it is somewhat inferior in quality if price is added, it is more advantageous in price difference than that.
This review is about item#37586762.
27 inch · dragonfly handle · used for single speed mummery
5
From Japan
On 2012-01-27 13:52:43
Since bags and bags such as bags and shopping bags are loaded in the wide size front basket (at the bottom at the basket allmesh), this one is used because the rattle falls at the time of parking on one foot stand. Even if it puts 10 - 15 kg on the front basket, it will not collapse. General Mamari Chari Balance Stand width 26 cm, this is excellent width stability 34 cm wide and 4 point grounding. Riding off the curb from the curbs on the sidewalk and riding on the road with curb stones, I rub on the feeling of one foot stand "Guri". Be careful who uses mummy calls on your rough. There is weight for minutes to be made sturdy. In the beginning you might feel that the pedal is rather heavy ~. I still do not know the durability. I think I will have one or two years even at commuting to school. I wonder if this price can be divided as consumable items.
This review is about item#37586771.
bicycle
1
From Japan
On 2011-06-13 15:47:14
When I inspected, there are some problems, returned by goods due to our inspection, for the following reasons. Pin bending, shaving, rivet caulking Inadequate We judged it as nonconforming standards by this and processed it.
This review is about item#37586762.
1
Customer Who Viewed This Item Also Viewed
Double Legged Stand, Bike Use
Long Carrier, Seat Stopper, Class 27
Bike Stand Parts
Type D Wire Baskets
Double Legged Stand, for Bicycle Use
Double Legged Stand, for Bicycle Use
Bike Stand Parts
Outer Double Stand
Bike Kickstand
Bike Kickstand
1 Side Kickstand
Double Side Stand