Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Brake Inner Wire Stainless Steel, For Both General And MTB Use

Brake Inner Wire Stainless Steel, For Both General And MTB Use
Sales Price: 3.99 SGD
Review Rating: 3.60
5 Customer Reviews
5 star 2
4 star 1
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
For myself
4
From Japan
On 2016-04-17 17:09:14
Because it does not rust it can ride with confidence
This review is about item#37600805.
Bicycle repair
5
From Japan
On 2015-11-12 15:04:32
Because the brakes' power is getting worse, purchase! Exchange went smoothly.
This review is about item#37600805.
Brake wire replacement / repair
5
From Japan
On 2013-11-08 22:36:00
When purchasing the same product of the same company in the past it was 1,700 mm indeed it was 1,600 mm whether there was a change in specification what we received this time. There was no problem as long as there was no need for that length under my use conditions, but those who purchase seeking the length are required to be careful. By the way it is Φ 1.6 mm as written by other reviewers since the previous specification. I knew that the brake lever side cap of Yoshikawa type · Yoshio type is attached and purchased because it is necessary but if it is not necessary, "ALLIGATOR (alligator) ATB / MTB brake inner cable" It is more advantageous.
This review is about item#37600805.
Brake wire repair
1
From Japan
On 2013-06-20 07:24:54
There was 1.5 mm in the item description, but the item that was sent was 1.6 mm. Although it is only 0.1 mm difference, it can not be used without matching the inner diameter of the outer. I would like you to list accurate information in item description. In addition, although there was nothing described in the explanation, since it was in a state with a drum, there is no description about presence or absence of a drum and size, so you can not see it for hands to sell on the net , I think that information on purchasers is insufficient.
This review is about item#37600805.
Bicycle brake wire
3
From Japan
On 2012-09-05 09:07:59
Exchange at the same time with the outer. The operation has become considerably lighter. Because there is no indication, I thought that the inner cap was not attached and I bought it separately, but it was attached to the product.
This review is about item#37600805.
1
Customer Who Viewed This Item Also Viewed
3S Wire
Standard Brake Cable Set
Brake Wire, City Bike
Bicycle Brake Wire Outer Cable
Brake Wire for Repair
Brake Wire for Repair
Brake Inner Wire
Brake Outer Cable
Brake Cable
Brake Cable
MTB SUS Blake Cable Set
ROAD SUS Blake Cable Set