Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of PTFE tube (10 m winding)

PTFE tube (10 m winding)
Sales Price: 7.99 SGD
Review Rating: 4.91
11 Customer Reviews
5 star 10
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
When installing the machine
5
From Japan
On 2018-04-23 22:07:40
It is a product not available in nearby home centers, very helpful! Delivery arrived in a few days, it was in time for the installation date!
This review is about item#37608417.
For stainless steel wire protection
5
From Japan
On 2017-12-14 15:05:21
For prototypes, it is very nice to purchase with a small amount of 10 m.
This review is about item#37608277.
For filament feed of 3D printer
5
From Japan
On 2017-07-30 15:26:49
I replaced it with what was attached at the time of 3D printer purchase. The filaments are delivered very smoothly and I am very satisfied.
This review is about item#37608331.
Used as a filler
5
From Japan
On 2017-07-13 14:43:33
It is easy to use, I think it is good. The price was not so high, so it was good.
This review is about item#37608347.
For stainless steel wire protection
5
From Japan
On 2015-06-19 16:00:05
Very satisfied because the price was cheap and the delivery was quick. Of course the goods were also satisfactory without particularly inconvenient places.
This review is about item#37608322.
Used as customer specified parts
5
From Japan
On 2015-06-09 11:06:12
There are no problems such as size variation and can be used stably.
This review is about item#37608322.
Insulation of electric wire
5
From Japan
On 2015-02-04 09:48:14
I love it as an insulator of electric wires for audio, and it demonstrates the best performance in all of high durability, strength, sound quality. When storing it may be broken if it is wound small. Although there is no split, the broken part becomes white and the mark remains. Be careful not to break when storing.
This review is about item#37608347.
Insulation
5
From Japan
On 2014-11-26 19:16:16
Because it uses only a small amount, we are saved 10 meters.
This review is about item#37608365.
Used for nozzles of 3D printers
5
From Japan
On 2014-10-13 19:04:30
It is a good product. I like it very much.
This review is about item#37608322.
Fabrication of special tool
5
From Japan
On 2014-01-17 11:04:37
Although the size was special, I almost gave up getting it, but when I searched for it by monotalou with "perhaps ..." ...! It is! It is really saved, because it will be 100 meters if customized. Besides it was cheap. Early, cheap, great! It is! Hopefully it is still better if PP tubes are of the same size.
This review is about item#37608313.
Crosslinked poly tap water for freezing steam ice
4
From Japan
On 2013-02-16 12:15:26
Heat resistant temperature goes smoothly into the pipe for 240 degrees
This review is about item#37608356.
1
Customer Who Viewed This Item Also Viewed
Silicone Tube
PTFE Tube, 1 M Roll
PFA Tube, 1 M Roll
Yodoflon PTFE Tube 6x4
PFA Tube, 10 M Roll
Fluorine Resin Tube, PFA
PFA Tubing, mm Size
Spaghetti tube
FEP Tubing
Twist tie PVC cut goods yellow
Naphron (R) BT tube (mm size)
PFA Tube
PTFE Tube