Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Power Transformer Single-Phase Winding 200V -> 100V

Power Transformer Single-Phase Winding 200V -> 100V
Sales Price: 44.49 SGD
Review Rating: 4.20
10 Customer Reviews
5 star 7
4 star 0
3 star 2
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Secure 100V power supply
3
From Japan
On 2017-09-28 18:15:11
Even though the power supply of the control equipment is 100 V, it is used for the control board which has only power 3 Φ 200 V. Literally convert from 200 V to 100 V. An inexpensive single volume was enough.
This review is about item#37649412.
Tractor Restore
5
From Japan
On 2016-02-08 19:12:35
It is a good seafood!
This review is about item#37649446.
Power supply for control equipment
1
From Japan
On 2015-03-11 20:28:05
When the equipment was connected to the secondary side 100 V terminal and 205 V was applied to the temporary side 200 V terminal, the voltage was confirmed as secondary side equipment was bad, 121 V was outputted. When rushing the temporary side to 220 V, the secondary side 100 V terminal output became 100 V. It was nearly destroying the equipment. If it is a normal voltage value, an instruction manual should be attached. Even at MADE IN JAPAN, I am dissatisfied that there is no manual or guarantee. Since there is no place to connect the ground, it would be appreciated if you could turn on the earth terminal.
This review is about item#37649421.
To use lighting of 100 V power supply overseas
5
From Japan
On 2015-02-02 08:47:55
I am satisfied because everything necessary for compact was attached.
This review is about item#37649437.
Down transformer inside the controller
5
From Japan
On 2014-12-18 17:38:51
Safety feeling used from before
This review is about item#37649421.
Since the power supply is only 200 volts,
5
From Japan
On 2014-11-27 17:38:03
It is very appreciated because it costs less than 100 volt power supply construction.
This review is about item#37649516.
At the time of solar installation.
5
From Japan
On 2014-07-19 08:52:57
It is a repeater. I am very satisfied.
This review is about item#37649412.
Used with single layer AC 100 V pump
5
From Japan
On 2014-07-13 15:22:41
It is carefully manufactured, the price is reasonable, and operation is satisfied satisfactorily without problems.
This review is about item#37649437.
Remote control device
5
From Japan
On 2014-05-01 19:56:06
It is light and outputs the secondary voltage accurately.
This review is about item#37649412.
To support the power supply voltage (200 V) to 100 V equipment
3
From Japan
On 2014-03-24 13:38:40
Since it is used by a customer (construction company), there is no particular problem, but there is no problem as there are terminals.
This review is about item#37649421.
1