Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Glass Scraper

Glass Scraper
Sales Price: 12.99 SGD
Review Rating: 4.78
9 Customer Reviews
5 star 8
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
Beauty
5
From Japan
On 2017-03-03 15:40:31
It is a standard item. Floor glass It is useful for every place such as kitchen dirt.
This review is about item#38107781.
Review correction
5
From Japan
On 2016-10-13 19:24:41
I wrote the same as the product of Narby but the thickness of the body is about 1.5 times thicker than Narby. Safety cover also has original cover completely different from Narby. If I get used to it, I do not think so, but Narby is lighter and thinner so it might be uncomfortable at first. On the contrary, because it has a thickness, it may be fine when peeling hard deposits. Although I do not know the one blade, it is the same thing as the thickness safety cover and Narby when purchasing it a few months ago. (There is no stamp on the main body)
This review is about item#38107797.
Removal of deposits of glass etc.
5
From Japan
On 2016-10-13 09:46:32
I am doing cleaning work at a hospital now while I am doing a former house cleaning. I sometimes do glass cleaning so this is a necessity item. Although I had a single blade, after all I bought this because the efficiency is bad if it is a single blade in a wide range. Although it sold also in Amazon, I got an inquiry, although it was almost the same price but made of the same Otsuka brush, the other side is that there is not a safety cover (cover attached to the blade). Purchasing on a standalone basis will not be stupid for about 800 yen if you put shipping costs. This is a conscience because it is attached and it is this price.
This review is about item#38107797.
Glass cleaning etc.
3
From Japan
On 2016-05-31 16:30:21
Unlike things that I used to date, there are thickness and weight. It becomes slightly hot, such as when you extend your arm to a high place and use it. I think that it is good if you can make it a little lightweight. I am glad that the cutting edge cover comes with it.
This review is about item#38107797.
It was Narby
5
From Japan
On 2016-03-23 13:17:18
Are you doing the same thing in Otsuka brush? I thought it was Narby. I was satisfied because I could buy a cheap price with a safety cover. This product is an essential item as I am cleaning work. I also have Escoglass Scraper, but I bought it because I got ugly because of acid burning. Esco is convenient as it can store blades with one touch. Just because you have a lock button on the part, you may touch the button while working and the blade may be stored. I used it even in the previous company (cleaning industry) but I bought it newly.
This review is about item#38107781.
Glass cleaning
5
From Japan
On 2015-08-16 02:27:10
It is very compact and I think that it is a good feeling for glass surface cleaning. Since all the corners of the handle part are sharp, we think that it can be used with confidence when using other files, such as file by scraping. Because the blade is a thin blade, it seems that it is not suitable for film peeling etc.
This review is about item#38107797.
Glass cleaning etc.
5
From Japan
On 2014-12-08 21:45:10
It is a very useful item, it is very easy to use. I will also purchase it.
This review is about item#38107781.
Cleaning the glass window
5
From Japan
On 2014-06-15 21:41:14
I am very happy with the cover
This review is about item#38107797.
Window cleaning, seal peeling
5
From Japan
On 2014-01-15 18:47:20
The cover of the blade part is glad about safety. About the fixation condition of replaceable replacement blade It was uneasy in the image, but it was enough strength without problems at all using the image.
This review is about item#38107781.
1
Customer Who Viewed This Item Also Viewed
Squeegee
Glass Scraper Blade
Blade Replacement Type Scraper
Sticker Scraper
Urethane Squeegee
Glass Scraper 200
Glass Scraper
G Scraper
Ankle processing apron
Scraper D Type