Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Wave Washer SUS

Wave Washer SUS
Sales Price: 6.99 SGD
Review Rating: 4.00
9 Customer Reviews
5 star 4
4 star 3
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
Improvement of motorcycle brake disk
5
From Japan
On 2018-02-24 10:00:47
I was thankful for being very cost effective.
This review is about item#38154426.
For motor bearing replacement
4
From Japan
On 2017-10-21 10:03:04
Wave washer of iron material has a perfect size for bearings, but I bought this for stainless steel materials but I wish it would be a little more rich in size. This is a bit small, so it's hard to incorporate it.
This review is about item#38154417.
Product assembly
1
From Japan
On 2017-06-09 14:38:57
The delivered actual item was φ9.6 in outer shape and 0.15 mm in thickness.
This review is about item#38154374.
Motorcycle disc rotor fixed
4
From Japan
On 2017-02-03 21:19:27
If it is used to fix the floating disk rotor to the hub, 3 point contact may be good. I think that it is the strength of Monotarou that such machine element parts can be easily obtained
This review is about item#38154392.
Machine maintenance
5
From Japan
On 2016-07-14 11:56:04
Nothing in particular. Quick correspondence. To be interested.
This review is about item#38154392.
As a substitute for the maker parts of the handle portion of the commercial washing machine
5
From Japan
On 2015-08-26 22:03:15
Because it is made of stainless steel at a price of 1/8 of the manufacturer's list price, it can be satisfactory enough.
This review is about item#38154435.
Unit assembly
3
From Japan
On 2014-11-25 08:43:47
I was looking for a compact and good stainless steel product so I could use it without problems
This review is about item#38154392.
Preventing the juncture from idling
5
From Japan
On 2013-02-09 19:14:09
I am using it without problems. It is easy to purchase if you can sell it in units of 10 pieces.
This review is about item#38154374.
WW-14_ When installing a bicycle pedal
4
From Japan
On 2012-09-26 00:37:39
It is used on the threaded bearing surface when installing the pedal to prevent scratches and galling of the crank. Because there is a reaction force in the washer itself, I think that it will also prevent loosening of screws. Since the inner diameter dimension is φ 14.5 (+ 0.3 / - 0.15), it is perfect for the thread of φ 9/16 inch (≈ φ 14.3).
This review is about item#38154426.
1