Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Small power relay G5Q

Small power relay G5Q
Sales Price: 1.99 SGD
Review Rating: 4.43
7 Customer Reviews
5 star 5
4 star 1
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Eco Cute repair
5
From Japan
On 2018-03-16 15:33:20
Case size and price We are satisfied with the current capacity.
This review is about item#39067874.
For adjusting the temperature of the seat heater
5
From Japan
On 2017-11-28 15:36:54
The consumption current of the coil is small and the control circuit can be simplified. It is tough for the board and I have never seen trouble. It is mediocre but excellent.
This review is about item#39067874.
Control of lighting etc.
5
From Japan
On 2017-05-17 07:42:17
It operates normally for several months. I use the copper wire instead of the foundation by soldering it to the terminal, I covered the terminal with a glue gun so that a force is applied to the terminal and it gets bent and does not break.
This review is about item#39067865.
To replace the power supply section relay in a narrow place
4
From Japan
On 2017-04-20 14:40:16
It was used for relocation of the power supply section in a narrow place, the processing was necessary with the universal base, but it was saved because only the monotalou was in the hand
This review is about item#39067822.
For magnet coil
5
From Japan
On 2016-11-16 14:29:28
I am satisfied with the case size and price and current capacity.
This review is about item#39067847.
For use on a motorcycle
5
From Japan
On 2016-10-21 00:05:38
I use it for 12 VDC as a bike, but I can use it normally.
This review is about item#39067847.
Contact point of small pump
2
From Japan
On 2015-09-07 18:03:45
It was cheap and the contact capacity was large, so it was cheap to use.
This review is about item#39067856.
1
Customer Who Viewed This Item Also Viewed
Power Relay G6B
Power Relay G5LE
Power Relay G5CA
Tsumekiri , Tsumayasurisetto
BPA series
Tsumeyasuri round type
TC4001BP (N, F)
Power Relay G6C
Power relay G5Q