Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of level for Plumbing artisan

 level for Plumbing artisan
Sales Price: 66.99 SGD
Review Rating: 3.25
4 Customer Reviews
5 star 1
4 star 1
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Drainage piping work
1
From Japan
On 2015-12-19 18:31:55
It is a structure that is very likely to cause errors in accuracy, and during use the fixing screws of the gradient bubble gauge will loosen enough to say all and the gradient will be incorrectly marked. The part which should not move absolutely moves easily. It will not be a business tool.
This review is about item#38640707.
Confirm gradient of external drainage piping
3
From Japan
On 2015-11-08 11:18:25
Basically it is a use premise for external work, it is always used in an environment where mud dirt adheres, but because notation such as gradient notation and upstream, downstream notation etc (gray character of black character base material) It is difficult to check on. I think that it is a good product if you can improve the notation matter a little more easily.
This review is about item#38640707.
Piping work
5
From Japan
On 2013-11-18 18:28:08
It was good for piping considering the gradient. People who do the piping work become aware of the gradient.
This review is about item#38640725.
Sewer piping work
4
From Japan
On 2013-05-19 22:19:33
First of all, I will do my fault. Since both ends of the cut end finish of aluminum were too sharp, I thought that as a finishing, I had to finish with a feeling of slightly dropping burrs and make it as smooth as the tool would be useless as a tool. The point that I bought was a short one so I thought that it was very easy to use because I bought one with two slopes of 1/100 and 1/50 with short construction. As an improvement point, when looking at the level of the actual mass, I used a horizontal instrument which is in the pocket behind the work pants or the waist bag, so I thought that it was hard to use unless it was made shorter. As a function to add, how about improving attaching a circle attached with a protractor on the back of the circle looking at the horizon etc of the mass so that various angles can be seen not only at the angle of 45 degrees but also at 45 degrees Is it? I am sorry for the selfish proposal, so I will use it as important because it is easy to use with the current leveling equipment. We sincerely ask you to develop wonderful tools ~
This review is about item#38638521.
1
Customer Who Viewed This Item Also Viewed
Pocket Slope Meter
Drainage Gradient Generator
Bubble Level
Blue Level for Gradient 450mm
Slope Level 2
Mobile Slope Level
Pocket Slope Meter
Slope gradient device
Spirit level Aiberu PT type
Pocket Level (with magnet)
 LEVEL GAUGE LUMINOUS CLASS WITH LED
Photo Scale