Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Bath Plug S Type

Bath Plug S Type
Sales Price: 11.51 SGD
Review Rating: 5.00
16 Customer Reviews
5 star 16
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 16 of 16 Reviews
Water heaters installation work
5
From Japan
On 2017-12-08 17:17:50
It is usually easy to use. It is cheaper than the things of other companies and it is saved.
This review is about item#38652731.
Hot water supply construction
5
From Japan
On 2017-10-18 12:37:42
It was used when changing from natural circulation to forced circulation. Installation is also simple and beautifully finished.
This review is about item#38652731.
Bath water heater attachment
5
From Japan
On 2017-06-02 22:22:12
I always ask you. The price is also cheap and saved.
This review is about item#38652731.
To the cap of the circulation port of the bathtub,
5
From Japan
On 2017-03-05 15:01:18
Because it is often done by one person, if you have this cap you can cap from the inside of the tub so convenient
This review is about item#38652731.
Close the hole in the bathtub
5
From Japan
On 2017-01-13 09:40:22
It was very easy to install. I think that it is good to describe how to remove the bathtub and bathtub and how to attach the bus cap to the item description.
This review is about item#38652731.
For closures
5
From Japan
On 2016-09-22 17:33:04
I closed the changed hole for hot water supply only.
This review is about item#38652731.
Hollow Bath Holder
5
From Japan
On 2016-08-16 17:14:50
Used to close the hole to keep medaka. It was completely closed and I could keep medaka safely
This review is about item#38652731.
Hole closure of overturning piping
5
From Japan
On 2016-07-07 20:06:04
There is a step in the rubber on the inside and it is a very good commodity that it can be put in the middle just because it enters the hole of 50 Φ.
This review is about item#38652731.
Fill in the bathtub.
5
From Japan
On 2016-07-03 13:37:09
Easy to install and convenient.
This review is about item#38652731.
Boiler installation
5
From Japan
On 2015-11-01 16:13:32
Easy to use
This review is about item#38652731.
Refurbishment of bath
5
From Japan
On 2015-02-10 08:12:34
Easy, it fits neatly.
This review is about item#38652731.
Because the kettle was broken ...
5
From Japan
On 2015-02-07 08:10:10
Since it can not add review articles, it will be the second review. I installed this after removing the broken kettle, but since useless melting of chill has become less likely, I got the right answer. The lid is also exchanged with a good feeling. Even during this period the remaining hot water is kept warm enough until next morning. Kami also w (^ o ^) w Should have done earlier.
This review is about item#38652731.
As intended
5
From Japan
On 2015-01-30 12:07:23
This product is not suitable for thin buses, such as sten, but attaching the venejam's empty lid to the board of about 10 mm of the board, open the hole 8 mm in the center and tighten together (rubber packing I applied a little silicone grease). There was a little curve on the bus side, but it was fixed with the driver alone, it was delicious without any leaks. It was cheaply accomplishable, it was frustrating.
Used as a cover for a two-hole bathtub
5
From Japan
On 2014-07-04 13:18:48
It was cheap and saved.
This review is about item#38652731.
Mecla in the bathtub
5
From Japan
On 2013-07-01 15:22:51
It was able to be used as usual with other goods.
This review is about item#38652731.
Hole closure in bathtub
5
From Japan
On 2012-09-17 13:44:57
Convenient because it can be tightened with a single driver from the inside.
This review is about item#38652731.
1
Customer Who Viewed This Item Also Viewed
Face Plug
Bath Screw Stop Plug
Plug for bus
Hot Water Supply Port Cover
Stainless Steel Bath Lid
Bus cosmetic lid
Hydrant Plug B
Pair Hose Parts Set
Pair Hose Circular Adapter
Circulation Adapter
Air Conditioner Pipe Cover
Bus in the tightening cosmetic lid
Bus in the tightening cosmetic lid
18-8 wok
Bath Screw Stop Plug