Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Sign board

Sign board
Sales Price: 0.99 SGD
Review Rating: 1.00
1 Customer Reviews
5 star 0
4 star 0
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 1 of 1 Reviews
A terminal block to be attached to the outer and inner covers of the small box to be placed in the control panel
1
From Japan
On 2017-12-03 22:02:46
Although it is made to fit in the groove of both ends because it was used for the 16P terminal block, it will fall immediately even if the board thickness is thinly inserted. Is the terminal block used for this general? Since it is a type that covers the part to fasten the screw with the crimp terminal rather than wiring at the upper and lower positions being used for it, there is no way to fix it and I used it by pasting it to the base part attaching the terminal board For the length it is good to pinch something in the middle, but because it is long for the thickness width it can not be fixed though it is exclusive You think that if it is a hard cover like a terminal cover safety cover you can insert it well but. . . .
This review is about item#75776276.
1
Customer Who Viewed This Item Also Viewed
Group Terminal Block Cover
Pvc Mark Sheets
Marking Plate
Terminal Block, PCB
One-touch terminal block WTB series
Jumper for operation tool
TJ-3A dedicated jack
Two stage cover
Dedicated Operation Tool
Rail End Stop
Sign board
Terminal Block ML-24
Registered Seal