Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Combination Spanner, Slim-Line

Combination Spanner, Slim-Line
Sales Price: -
Review Rating: 4.17
6 Customer Reviews
5 star 3
4 star 1
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Car maintenance
5
From Japan
On 2017-04-04 23:23:35
It was easy to use normally. I do not know without using more durability.
This review is about item#39214524.
Citi cycle maintenance
5
From Japan
On 2016-04-25 22:32:00
It was thin, light, handled comfortably, none of the nuts were licked. I am satisfied because the price was good and the quality was good. Usage goals are compatible In case of rear wheel attachment and detachment of a city cycle with a stand, I think that you can work with stress without using a ratchet or a deep socket. (Since the stand interfered slightly when it was using a straight combination in a situation where the hand fastening of the nut was not possible so much and it was not able to rotate more than 180 degrees)
This review is about item#39214542.
Car maintenance
3
From Japan
On 2015-12-22 02:17:48
It is quite thin, so it can be used in a narrow place where ordinary wrenches do not enter. Because it is cheap, it seems to be good if there are all sizes.
This review is about item#39214524.
General work
4
From Japan
On 2015-02-14 19:25:54
There was no particular problem and the texture was a favorite thing. I guess it will slip a bit.
This review is about item#39214524.
Bicycle maintenance
5
From Japan
On 2014-06-13 21:24:02
Because there was no size in the accessory spanner, we purchased for 10 mm and 15 mm for the first time as a spanner alone, but the fact that the basic performance as a tool is solid is originally more beautiful in design and finish, As I saw it. I would like to arrange other sizes as necessary.
This review is about item#39214497.
Maintenance of private cars
3
From Japan
On 2013-06-16 19:08:16
Those of an unnamed brand that I bought at a home center are badly purchased because they are out of accuracy. Although there was no problem in use, there were scratches on the mouth portion that there was burr and there was scratch on the satin finishing finish. The accuracy is good and it is cheap, so there is no problem. It is a point to worry about finish being sweet compared to Proxon 10 years ago. If you are the first purchaser you may not mind.
This review is about item#39214515.
1
Customer Who Viewed This Item Also Viewed
Combination spanner
Combination Wrench
Combination wrench
Combination wrench
Combination spanner
CP Combination Wrench Long Type
Combination wrench
CL Combination Wrench
Combination wrench
Combination Wrench CP
One eye-box wrench
The new combination spanner
The new combination spanner inch size