Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Brake Pads

Brake Pads
Sales Price: 13.88 SGD
Review Rating: 4.83
12 Customer Reviews
5 star 10
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 12 of 12 Reviews
Purchase for motorcycle maintenance
5
From Japan
On 2017-05-06 18:23:07
Although I have not used it yet because I purchased it to spare, the feeling I saw is firm and has a good feeling.
This review is about item#39279913.
Replacement of consumable parts
5
From Japan
On 2016-11-28 15:04:36
It is installed and used without change as a genuine product. Efficiency does not differ much but it is several tens of kilometers after exchange, but I do not feel the problem. Since I was using over 10,000 kilos on the genuine pad of a new car, I think that it would be better if I could use the same degree.
This review is about item#39279913.
driving
5
From Japan
On 2016-11-03 23:18:14
Anyway, it cheaply gotten in. I will purchase it again.
This review is about item#39279922.
ATV exchange
5
From Japan
On 2016-10-19 17:56:30
Unqualified unari, buggy, but it was attached without problem.
This review is about item#39279922.
Replacing the front brake pad
5
From Japan
On 2016-06-20 17:57:17
Since it was the first pad exchange, I heard the tricks for the bike shop going home so it is now safe without cutting noise on the back of the pad and chamfering of the pad as it is improving the accuracy of the work. It is! Even though I decided to do that, it did not cry. There is no way this performance complaint can be attached at this price! It is!
This review is about item#39279913.
Address V 125
5
From Japan
On 2016-04-05 18:21:23
When running, the difference with genuine products is not understood by amateurs.
This review is about item#39279913.
Two wheel drive
5
From Japan
On 2016-02-25 19:16:40
It does not change with genuine products
This review is about item#39279913.
Used in PCX
4
From Japan
On 2015-09-26 05:56:01
From the beginning of use, we used about 3,000 km for 4 months. I think that the effect is almost the same as genuine. I was thinking to chamfer a little since I started singing around this time. I think that this is good because there are few go-stops in commuting main. The price is also satisfactory.
This review is about item#39279886.
Live Dio
4
From Japan
On 2015-02-17 14:13:10
cheap. I do not know the difference with genuine.
This review is about item#39279904.
For commuter motorcycles
5
From Japan
On 2014-07-04 05:42:09
The price was not expensive, it saved me the trouble of going to buy immediately after ordering. Although goods are not called high quality, I am satisfied nearly pure. I also want to buy next.
This review is about item#39279913.
As a replacement part of the pad
5
From Japan
On 2013-02-25 13:57:42
Price, braking power, no problem. Durability seems to be good.
This review is about item#39279913.
Exchange from genuine pad
5
From Japan
On 2012-11-15 18:08:45
Address V 125 S Because it changed to a large diameter rotor or 6000 km, the remaining amount of the pad became about 1.5 mm so we chose this product The braking power is not inferior compared to genuine cost performance is the best
This review is about item#39279913.
1
Customer Who Viewed This Item Also Viewed
Brake Pad, Golden Pad
Brake Pad, Hyper Pad
Disc Plate
MEGA ALLOY X PAD Sintered
Brake Pad
Brake Pads
Brake Pad
Non Fade Brake Shoe
Hyper Sintered
scooter
Brake Pad