Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Unika Adhesive Anchor Resin A, Infution Type GE-410

Unika Adhesive Anchor Resin A, Infution Type GE-410
Sales Price: 34.99 SGD
Review Rating: 3.00
2 Customer Reviews
5 star 1
4 star 0
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 2 of 2 Reviews
Used for anchoring work on the floor for permeation prevention.
5
From Japan
On 2017-05-22 14:38:48
It is convenient to use if you replace the tip cartridge next time even if it is surplus because it is two liquid type. I used it in a commercial caulking gun, but a product of a large size is caution not to be able to extract two liquids without "special cancer".
This review is about item#36593435.
Chemical anchor
1
From Japan
On 2015-08-18 18:05:32
Unlike the bin type, I choose a bolt size very well so I think it is a very good product, but I really care about the use in the summer. Last year I tried to use it in the summer in the summer, so I could not use it in a fixed inside. I had the opportunity to use it in the summer this year, using care and storing it at a cold dark place immediately, put it in the cooler box on the scene, but ... but because the central part got settled, it can not be used. It can only be thought that it got warmed and cured among logistics until ordering and delivering (just because it was a hot day). Should I buy two bottle types to prevent it ... as I did it, it seems to settle down to old-fashioned bin type after all. Because you can not use products with Atari loser brought to the site with a brand new, I will not buy it anymore.
This review is about item#39448281.
1
Customer Who Viewed This Item Also Viewed
Ea-500, Resin Sets
EA-500 (base kit)
EL350 Cartridge
EA-500S Dispenser
Eborokku GL450
Mixing Nozzle
Resin A injection gun
Chemical Anchor Kit