Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Collet

Sales Price: 34.99 SGD
Review Rating: 4.00
1 Customer Reviews
5 star 0
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 1 of 1 Reviews
Polishing of places that can not be done with ordinary grinders
From Japan
On 2013-09-05 08:05:06
There is something that MGS 38A has the same model number and the specification is different, and this collet is corresponded only to recent models, there are things that can not be used for the old type of aluminum as a whole body. be careful. Originally I was not able to use it because it was old type, so it was originally evaluated as "dissatisfied", but the person who supported the negotiation to the manufacturer side worked hard and I am very grateful that it is possible to purchase expendable parts, so that based on that We will make this evaluation. Although acceptance was prompt, it was regrettable that we could not move until we asked for a situation confirmation from here without a moment, so the system improvement on that point and the 3 mm axis which seems to be equivalent to this product I would like to have a statement of attention to the description of the type of item.
This review is about item#39465221.
Customer Who Viewed This Item Also Viewed
Micro Grinder Collet Chuck
Micro Grinder Collet Chuck
Collet for air micro grinder
Die Grinder
Collet chuck for straight grinder
Internal grinding wheel
Collet 3 for Mitachi straight