Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Jigsaw Blade Ironwork

Jigsaw Blade Ironwork
Sales Price: 24.99 SGD
Review Rating: 4.50
2 Customer Reviews
5 star 1
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 2 of 2 Reviews
Square hole of board, pipe cut at site.
5
From Japan
On 2017-04-18 22:38:24
It is possible to cut at a higher speed than the blade you have been using. I also feel that the life span is long. I tried cutting the pipe (SGP) cutting as well. Up to 40 A can be cut without problems. (I have not tried more than 50 A) It is a level that is slow although it is slow compared to a high-speed cutting machine, but it is slightly difficult to put out a right angle. It may be a suitable tool next to the sapphire saw in the case of permission application or disconnection at troublesome places where using a high speed cutting machine is troublesome. (Place where complaints are also complicated by Thunder's cutting blade) (I think that sappersaw is better ... but I do not have it, so I do not know it.)
This review is about item#39471625.
Used for cutting 30t blocks of material A 5083
4
From Japan
On 2017-02-20 18:06:14
Although it was also good to use a band sawing machine, it costs expenses when breaking the cutlery, so I tried using it to cut thick objects, but the sharpness was good and the possibilities of jigsaw spread.
This review is about item#39471625.
1
Customer Who Viewed This Item Also Viewed
Jigsaw Blade
Jigsaw Blade
Jigsaw blade
Jigsaw Blade
Jigsaw Blade
Jigsaw (Bosch type)
Jigsaw Blade
3 jigsaw blades